<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx28evk and eth1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181902#M7869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello all-&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the i.MX28EVK, and I'm having a hard time bringing up the second NIC consistently. I initially ran into this was the ltib build I made, but then I grabbed the included Linux SD card, and it results in the same behavior. The frustrating thing is that every 4-5 boots or so it works (using the reference image), but the rest of the time it doesn't. When it doesn't work, I get the following in the serial session (from the reference image marked "MX28EVK Linux 110-77224 Rev c"):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/***********************/&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;eth1: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Down&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Down&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/***********************/&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought for a while that it might be a hardware issue, but the the Windows CE reference build works every time I boot it. Any suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Nov 2011 18:50:15 GMT</pubDate>
    <dc:creator>CH1z</dc:creator>
    <dc:date>2011-11-01T18:50:15Z</dc:date>
    <item>
      <title>imx28evk and eth1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181902#M7869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello all-&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the i.MX28EVK, and I'm having a hard time bringing up the second NIC consistently. I initially ran into this was the ltib build I made, but then I grabbed the included Linux SD card, and it results in the same behavior. The frustrating thing is that every 4-5 boots or so it works (using the reference image), but the rest of the time it doesn't. When it doesn't work, I get the following in the serial session (from the reference image marked "MX28EVK Linux 110-77224 Rev c"):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/***********************/&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;eth1: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Down&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Down&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/***********************/&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought for a while that it might be a hardware issue, but the the Windows CE reference build works every time I boot it. Any suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2011 18:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181902#M7869</guid>
      <dc:creator>CH1z</dc:creator>
      <dc:date>2011-11-01T18:50:15Z</dc:date>
    </item>
    <item>
      <title>Re: imx28evk and eth1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181903#M7870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Forgot to mention, eth0 comes up fine in all cases, just eth1 that is troublesome&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2011 19:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181903#M7870</guid>
      <dc:creator>CH1z</dc:creator>
      <dc:date>2011-11-01T19:17:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx28evk and eth1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181904#M7871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having this same issue. I'm testing with the standard 2.6.35 images from Freescale, booting from 4 GB SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I boot the board, and then log-in via the debug serial port. To start eth0 and eth1, I issue the commands:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;udhcpc -b -i eth0&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;udhcpc -b -i eth1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have two imx28evk boards. On one board, it works fine. On the other board, eth0 works, but eth1 endlessly prints:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Down&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Down&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Down&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Down&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Down&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;PHY: 0:01 - Link is Down&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LEDs flash momentarily, periodically, which isn't the behaviour of the functional board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be different between the functional board and the non-functional board? Both boards have stickers saying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;700-26241 REV A&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;SCH-26241 REV D&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2012 06:57:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181904#M7871</guid>
      <dc:creator>CraigMcQueen</dc:creator>
      <dc:date>2012-09-18T06:57:47Z</dc:date>
    </item>
    <item>
      <title>Re: imx28evk and eth1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181905#M7872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://groups.google.com/forum/#!topic/meta-fsl-arm/eQW7vTobZ00" title="https://groups.google.com/forum/#!topic/meta-fsl-arm/eQW7vTobZ00"&gt;https://groups.google.com/forum/#!topic/meta-fsl-arm/eQW7vTobZ00&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had the same problem... Had to move to a new kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2012 18:58:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28evk-and-eth1/m-p/181905#M7872</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2012-09-18T18:58:26Z</dc:date>
    </item>
  </channel>
</rss>