<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6 battery boot problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-battery-boot-problem/m-p/490638#M78658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have boot problems in SABRE SD platform after halting system while having LICELL pin connected to a coin cell battery (BT500 connector in SABRE SD platform).&lt;/P&gt;&lt;P&gt;The steps we have followed are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Connect a coin cell battery to BT500 SABRE SD platform connector.&lt;/LI&gt;&lt;LI&gt;Switch SABRE SD platform board on.&lt;/LI&gt;&lt;LI&gt;Boot linux and enter commands to refresh date:&lt;UL&gt;&lt;LI dir="ltr"&gt;date -s '2016-04-27 18:34:00'&lt;/LI&gt;&lt;LI dir="ltr"&gt;hwclock -w&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI dir="ltr"&gt;Enter halt command:&lt;UL&gt;&lt;LI dir="ltr"&gt;halt&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI dir="ltr"&gt;Switch SABRE SD platform board off and on.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;After following these steps we are not able to boot the SABRE SD platform anymore. To be able to boot the board, we have to disconnect the coin cell battery.&lt;/P&gt;&lt;P&gt;If step 4 is not applied (no halt command is introduced) we have no booting problems.&lt;/P&gt;&lt;P&gt;Why are we having this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Apr 2016 12:37:23 GMT</pubDate>
    <dc:creator>joseporga</dc:creator>
    <dc:date>2016-04-29T12:37:23Z</dc:date>
    <item>
      <title>iMX6 battery boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-battery-boot-problem/m-p/490638#M78658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have boot problems in SABRE SD platform after halting system while having LICELL pin connected to a coin cell battery (BT500 connector in SABRE SD platform).&lt;/P&gt;&lt;P&gt;The steps we have followed are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Connect a coin cell battery to BT500 SABRE SD platform connector.&lt;/LI&gt;&lt;LI&gt;Switch SABRE SD platform board on.&lt;/LI&gt;&lt;LI&gt;Boot linux and enter commands to refresh date:&lt;UL&gt;&lt;LI dir="ltr"&gt;date -s '2016-04-27 18:34:00'&lt;/LI&gt;&lt;LI dir="ltr"&gt;hwclock -w&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI dir="ltr"&gt;Enter halt command:&lt;UL&gt;&lt;LI dir="ltr"&gt;halt&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI dir="ltr"&gt;Switch SABRE SD platform board off and on.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;After following these steps we are not able to boot the SABRE SD platform anymore. To be able to boot the board, we have to disconnect the coin cell battery.&lt;/P&gt;&lt;P&gt;If step 4 is not applied (no halt command is introduced) we have no booting problems.&lt;/P&gt;&lt;P&gt;Why are we having this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 12:37:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-battery-boot-problem/m-p/490638#M78658</guid>
      <dc:creator>joseporga</dc:creator>
      <dc:date>2016-04-29T12:37:23Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 battery boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-battery-boot-problem/m-p/490639#M78659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Looks like, the problem relates to PMIC settings after Linux "halt" command,&lt;/P&gt;&lt;P&gt;which do not allow to start-up system : full POR reset is needed (to return default&lt;/P&gt;&lt;P&gt;PMIC configuration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 04:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-battery-boot-problem/m-p/490639#M78659</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-05-03T04:28:24Z</dc:date>
    </item>
  </channel>
</rss>