<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q Enet Cannot Reach 1000M</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Enet-Cannot-Reach-1000M/m-p/490537#M78633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a known issue. Please read the "Chip Errata for the i.MX 6" and look for the ERR004512:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps.&lt;/LI&gt;&lt;LI&gt;Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to 1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher than 400 Mbps, there is a risk of ENET RX FIFO overrun.&lt;/LI&gt;&lt;LI&gt;There is no workaround for the throughput limitation.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Feb 2016 09:50:31 GMT</pubDate>
    <dc:creator>gary_bisson</dc:creator>
    <dc:date>2016-02-05T09:50:31Z</dc:date>
    <item>
      <title>IMX6Q Enet Cannot Reach 1000M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Enet-Cannot-Reach-1000M/m-p/490536#M78632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone help me? in my MX6Q custom board based on MX6QSD(imx_3.0.35_4.1.0), our 1GB RGMII ethernet can only work at speed 495Mbits/sec,&lt;/P&gt;&lt;P&gt;is this normal ? Which configuration will affect the speed？&lt;/P&gt;&lt;P&gt;=============================================&lt;/P&gt;&lt;P&gt;iperf -c 192.168.122.125 -u -b 800M -t 10 -l 1000&lt;/P&gt;&lt;P&gt;------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Client connecting to 192.168.122.125, UDP port 5001&lt;/P&gt;&lt;P&gt;Sending 1000 byte datagrams&lt;/P&gt;&lt;P&gt;UDP buffer size:&amp;nbsp; 208 KByte (default)&lt;/P&gt;&lt;P&gt;------------------------------------------------------------&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 3] local 192.168.122.6 port 45130 connected with 192.168.122.125 port 5001&lt;/P&gt;&lt;P&gt;[ ID] Interval&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Transfer&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bandwidth&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 3]&amp;nbsp; 0.0-10.0 sec&amp;nbsp;&amp;nbsp; 590 MBytes&amp;nbsp;&amp;nbsp; 495 Mbits/sec&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 3] Sent 618437 datagrams&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 3] WARNING: did not receive ack of last datagram after 10 tries.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 02:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Enet-Cannot-Reach-1000M/m-p/490536#M78632</guid>
      <dc:creator>javen</dc:creator>
      <dc:date>2016-02-05T02:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q Enet Cannot Reach 1000M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Enet-Cannot-Reach-1000M/m-p/490537#M78633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a known issue. Please read the "Chip Errata for the i.MX 6" and look for the ERR004512:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps.&lt;/LI&gt;&lt;LI&gt;Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to 1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher than 400 Mbps, there is a risk of ENET RX FIFO overrun.&lt;/LI&gt;&lt;LI&gt;There is no workaround for the throughput limitation.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 09:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Enet-Cannot-Reach-1000M/m-p/490537#M78633</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2016-02-05T09:50:31Z</dc:date>
    </item>
  </channel>
</rss>