<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to rebuild package like gpsd by using yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-rebuild-package-like-gpsd-by-using-yocto/m-p/490438#M78605</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the enclosed file, focus on the chapter 1.3 Customizing the i.MX 6 or i.MX 7 Custom Board Code&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Mar 2016 07:49:26 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2016-03-24T07:49:26Z</dc:date>
    <item>
      <title>How to rebuild package like gpsd by using yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-rebuild-package-like-gpsd-by-using-yocto/m-p/490437#M78604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm trying to make an image by using yocto.&lt;/P&gt;&lt;P&gt;And some packages such as gpsd, nfs, etc are added into my file system.&lt;/P&gt;&lt;P&gt;Additionally, I'd like to modify some source code related to gpsd in the blow path&lt;/P&gt;&lt;P&gt;and rebuild only gpsd and make a root file system including the modified gpsd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gpsd source code path in yocto : &lt;/P&gt;&lt;P&gt;/fsl-community-bsp-daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gpsd/3.14-r0/gpsd-3.14&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, I modified gpsd source code and run bitbake as the following procedure. &lt;/P&gt;&lt;P&gt;- bitbake gpsd&lt;/P&gt;&lt;P&gt;- make a image and file system including gpsd by using hob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there any missing procedure for making image including a modified gpsd?&lt;/P&gt;&lt;P&gt;Could anyone give some idea for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Mar 2016 00:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-rebuild-package-like-gpsd-by-using-yocto/m-p/490437#M78604</guid>
      <dc:creator>kimhansung</dc:creator>
      <dc:date>2016-03-21T00:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to rebuild package like gpsd by using yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-rebuild-package-like-gpsd-by-using-yocto/m-p/490438#M78605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the enclosed file, focus on the chapter 1.3 Customizing the i.MX 6 or i.MX 7 Custom Board Code&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Mar 2016 07:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-rebuild-package-like-gpsd-by-using-yocto/m-p/490438#M78605</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-03-24T07:49:26Z</dc:date>
    </item>
  </channel>
</rss>