<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Booting i.MX6 Android from NOR FLASH in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490407#M78594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the responses, but none really address the question of how to use BOOTA with NOR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After much digging, there is a way to implement this.&amp;nbsp; BOOTA takes an address as a parameter.&amp;nbsp; So, if a BOOT.IMG is programmed into flash at say address 0x08080000, I can use the U-Boot command BOOTA 0x08080000 to correctly load this image and boot...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps someone else....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 May 2016 16:17:03 GMT</pubDate>
    <dc:creator>mike_sims</dc:creator>
    <dc:date>2016-05-26T16:17:03Z</dc:date>
    <item>
      <title>Booting i.MX6 Android from NOR FLASH</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490405#M78592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have questions about booting Android from NOR on a Sabre AI (imx6dl CPU2) board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am preparing a SW Build for our custom HW design by using the SabreAI board.&amp;nbsp;&amp;nbsp; I have built the sw provided by NXP to boot Android from SD Card (this works well).&amp;nbsp; I am trying to adapt this SW to put u-boot and the boot image on the on-board 32MB NOR, but I do not see a way in U-Boot to use BOOTA from NOR.&amp;nbsp;&amp;nbsp; Is U-Boot the right bootloader to use to boot from NOR??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For now, I am OK with having the remaining partitions on SD Card.&amp;nbsp; In our custom application, I would want the boot, bootimage, recoveryimage, and system partition on NOR.&amp;nbsp;&amp;nbsp; Will I need to modify the FSTAB, INIT*.RC, or System Image to move these partitions from SD to NOR??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your answers...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 May 2016 20:20:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490405#M78592</guid>
      <dc:creator>mike_sims</dc:creator>
      <dc:date>2016-05-21T20:20:20Z</dc:date>
    </item>
    <item>
      <title>Re: Booting i.MX6 Android from NOR FLASH</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490406#M78593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Arial',sans-serif; font-size: 10pt;"&gt;Android MM6.0 release doc , for SabreAI board , boot source tested are :&lt;SPAN class="c0"&gt;External SD and NAND.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Arial',sans-serif; font-size: 10pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black; font-size: 10pt; font-family: 'Arial',sans-serif;"&gt;For Linux 4.1.15 release note , there is u-boot&amp;nbsp; configure for SabreAI board boot from nor flash.&amp;nbsp; Re&lt;/SPAN&gt;&lt;SPAN style="color: black; font-family: 'Arial',sans-serif; font-size: 10pt;"&gt;fer it to generate u-boot which could boot from NOR flash.&amp;nbsp; For&lt;/SPAN&gt;&lt;SPAN style="color: black; font-family: 'Arial',sans-serif; font-size: 10pt; mso-fareast-font-family: Calibri; mso-fareast-theme-font: minor-latin; mso-ansi-language: EN-US; mso-fareast-language: EN-US; mso-bidi-language: AR-SA;"&gt; Kernel and other image storage partitions, one could take the android release user guide doc. for reference.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 11:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490406#M78593</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2016-05-25T11:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: Booting i.MX6 Android from NOR FLASH</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490407#M78594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the responses, but none really address the question of how to use BOOTA with NOR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After much digging, there is a way to implement this.&amp;nbsp; BOOTA takes an address as a parameter.&amp;nbsp; So, if a BOOT.IMG is programmed into flash at say address 0x08080000, I can use the U-Boot command BOOTA 0x08080000 to correctly load this image and boot...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps someone else....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2016 16:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-i-MX6-Android-from-NOR-FLASH/m-p/490407#M78594</guid>
      <dc:creator>mike_sims</dc:creator>
      <dc:date>2016-05-26T16:17:03Z</dc:date>
    </item>
  </channel>
</rss>