<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX233 package variants</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490394#M78589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. no&lt;/P&gt;&lt;P&gt;2. HW_CLKCTRL_ETM can be considered as reserved, &lt;/P&gt;&lt;P&gt;HW_CLKCTRL_PIX is functional, since LQFP128 supports&lt;/P&gt;&lt;P&gt;ITU-R BT.656 8-bit+clock mode according to Table 1-1. i.MX23 &lt;/P&gt;&lt;P&gt;Functions by Package&amp;nbsp; i.MX23 RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Apr 2016 01:33:14 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-04-11T01:33:14Z</dc:date>
    <item>
      <title>i.MX233 package variants</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490393#M78588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have some questions about the i.MX233 package variants:&lt;/P&gt;&lt;P&gt;1. Is it possible to identify the the package variant (LQFP128, BGA169) of the i.MX233 via register?&lt;/P&gt;&lt;P&gt;2. How should be HW_CLKCTRL_ETM and HW_CLKCTRL_PIX treat on LQFP128?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Apr 2016 09:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490393#M78588</guid>
      <dc:creator>lategoodbye</dc:creator>
      <dc:date>2016-04-09T09:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 package variants</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490394#M78589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. no&lt;/P&gt;&lt;P&gt;2. HW_CLKCTRL_ETM can be considered as reserved, &lt;/P&gt;&lt;P&gt;HW_CLKCTRL_PIX is functional, since LQFP128 supports&lt;/P&gt;&lt;P&gt;ITU-R BT.656 8-bit+clock mode according to Table 1-1. i.MX23 &lt;/P&gt;&lt;P&gt;Functions by Package&amp;nbsp; i.MX23 RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 01:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490394#M78589</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-11T01:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 package variants</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490395#M78590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now i'm a little bit confused. According to i.MX23 reference manual chapter 6.4.2 there should be a register to identify the package variant (HW_DIGCTL_STATUS_PACKAGE_TYPE, 0=BGA, 3=LQFP), which is also in the bootlet code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 19:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490395#M78590</guid>
      <dc:creator>lategoodbye</dc:creator>
      <dc:date>2016-06-08T19:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 package variants</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490396#M78591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are right, sorry I missed that:&lt;/P&gt;&lt;P&gt;HW_DIGCTL_STATUS[PACKAGE_TYPE]:&amp;nbsp; package type. 000=169BGA, 011=128TQFP&lt;/P&gt;&lt;P&gt;Table 6-4. HW_DIGCTL_STATUS i.MX23 Reference Manual (rev.1, 11/2009).&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Ffiles%2Fdsp%2Fdoc%2Fref_manual%2FIMX23RM.pdf" rel="nofollow" target="_blank"&gt;http://www.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2016 01:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-package-variants/m-p/490396#M78591</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-09T01:09:22Z</dc:date>
    </item>
  </channel>
</rss>