<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: GENIVI 7.0 With Qt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489438#M78457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nirmal T M,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you adding the meta-ivi layer on top of one of NXPs BSPs? How did you added the Qt layer to your environment?&lt;/P&gt;&lt;P&gt;It looks from the readme on the meta-ivi layer that the intrepid-image does not have additional dependencies other than poky and meta-openembedded. Although it seems that there is a qt4 append recipe inside this layer. I would recommend looking at it and seeing if you may add it to this image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is some information on integrating GENIVI to a Qt distribution on the web, like the presentation below, but it only gives general guidelines.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.youtube.com/watch?v=sWas9HIOyNc"&gt;https://www.youtube.com/watch?v=sWas9HIOyNc&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 May 2016 20:46:21 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-05-03T20:46:21Z</dc:date>
    <item>
      <title>GENIVI 7.0 With Qt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489437#M78456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I am trying to build GENIVI 7.0 (intrepid-image) using Yocto Build Procedure for iMX6 SABREE AI. The Genivi Build was successful, But i need to add Qt Layer to this. So i added the QT in bb layer of yocto build. but the resulted Intrepid-image does not contain any part of Qt.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is it possible for building (yocto) intrepid-image with Qt ??&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;what bitbake command I need to use. kindly help me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 10:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489437#M78456</guid>
      <dc:creator>nirmaltm</dc:creator>
      <dc:date>2016-04-29T10:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: GENIVI 7.0 With Qt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489438#M78457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nirmal T M,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you adding the meta-ivi layer on top of one of NXPs BSPs? How did you added the Qt layer to your environment?&lt;/P&gt;&lt;P&gt;It looks from the readme on the meta-ivi layer that the intrepid-image does not have additional dependencies other than poky and meta-openembedded. Although it seems that there is a qt4 append recipe inside this layer. I would recommend looking at it and seeing if you may add it to this image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is some information on integrating GENIVI to a Qt distribution on the web, like the presentation below, but it only gives general guidelines.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.youtube.com/watch?v=sWas9HIOyNc"&gt;https://www.youtube.com/watch?v=sWas9HIOyNc&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 20:46:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489438#M78457</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-05-03T20:46:21Z</dc:date>
    </item>
    <item>
      <title>Re: GENIVI 7.0 With Qt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489439#M78458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks gusarambula,&lt;/P&gt;&lt;P&gt;Previously I have given my DISTRO option as "poky-ivi-systemd" and I have added the meta-qt layer on &lt;STRONG&gt;bblayers&lt;/STRONG&gt; at that time the genivi image have successfully build (with out qt component). but when i changed the DISTRO to "fsl-ivi-vfb" which end up with build error.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;so I understand that while building GENIVI on yocto as "intrepid-image" does not have any qt options.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there any other bitbake image which can be used to build both GENIVI and QT layer together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At present I am cross compile Qt 5.5 for the yocto build GENIVI image for my iMX6 Sabree Ai board with GENIVI 7.0.3 (intrepid-image) File System. Also I have installed the EGLFS Libraries in the GENIVI file system. while configuring the Qt for cross compile I received the following error.&lt;/P&gt;&lt;P&gt;his is the Qt Open Source Edition.&lt;/P&gt;&lt;P&gt;You are licensed to use this software under the terms of&lt;BR /&gt; the Lesser GNU General Public License (LGPL) versions 2.1.&lt;BR /&gt; You are also licensed to use this software under the terms of&lt;BR /&gt; the GNU Lesser General Public License (LGPL) versions 3.&lt;/P&gt;&lt;P&gt;You have already accepted the terms of the Open Source license.&lt;/P&gt;&lt;P&gt;&amp;lt;srcbase&amp;gt; = /media/acs/f64c24ce-b50c-4395-bb84-429476e2905a/static-qt-new/qt5/qtbase&lt;BR /&gt; &amp;lt;outbase&amp;gt; = /media/acs/f64c24ce-b50c-4395-bb84-429476e2905a/static-qt-new/qt5/qtbase&lt;BR /&gt; Creating qmake...&lt;BR /&gt; ..Done.&lt;BR /&gt; Running configuration tests...&lt;BR /&gt; Warning: Disabling pkg-config since PKG_CONFIG_LIBDIR is not set.&lt;BR /&gt; Note: PKG_CONFIG_SYSROOT_DIR automatically set to /home/acs/Downloads/L3.14.52_1.1.0-ga_images_MX6QDLSOLO/fsl-image-gui-fb-imx6qdlsolo&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could not determine the target architecture!&lt;/STRONG&gt;&lt;BR /&gt; Turn on verbose messaging (-v) to see the final report.&lt;BR /&gt; &lt;STRONG&gt;The OpenGL ES 2.0 functionality test failed!&lt;/STRONG&gt;&lt;BR /&gt; Use of pkg-config is not enabled, maybe you want to pass -force-pkg-config?&lt;BR /&gt; You might need to modify the include and library search paths by editing&lt;BR /&gt; QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in&lt;BR /&gt; /media/acs/f64c24ce-b50c-4395-bb84-429476e2905a/static-qt-new/qt5/qtbase/mkspecs/devices/linux-imx6-g++.&lt;/P&gt;&lt;P&gt;I have used the gcc-linaro-5.2-2015.11-1-x86_64_arm-linux-gnueabihf-g++ as a cross compile tool chain&lt;/P&gt;&lt;P&gt;Is it possible to clear this error.&lt;BR /&gt; I need to build the Qt with EGL support,&lt;BR /&gt; Kindly help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 05:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489439#M78458</guid>
      <dc:creator>nirmaltm</dc:creator>
      <dc:date>2016-05-06T05:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: GENIVI 7.0 With Qt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489440#M78459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nirmal ,&lt;/P&gt;&lt;P&gt;Could you please share me the steps which you followed for the genivi&amp;nbsp; build ? which yocto package you are using how can add &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; meta-ivi layer on&amp;nbsp; yocto package.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sachu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 10:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GENIVI-7-0-With-Qt/m-p/489440#M78459</guid>
      <dc:creator>sachusanal</dc:creator>
      <dc:date>2016-07-14T10:03:39Z</dc:date>
    </item>
  </channel>
</rss>