<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Update kernel modules in image recipe</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Update-kernel-modules-in-image-recipe/m-p/489391#M78453</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Durmus,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m afraid I’m not aware or any easy way to update the kernel modules contained in on your custom image to that they match the kernel config file. I’m not sure if working on a kernel configuration based on the current kernel of the image is an option but either way it will be a bit time consuming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 May 2016 21:23:51 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-05-03T21:23:51Z</dc:date>
    <item>
      <title>Update kernel modules in image recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Update-kernel-modules-in-image-recipe/m-p/489390#M78452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I created a custom image recipe using hob. I took qt4e-demo-image as a reference and added some packages and removed others. Then I saved it in &lt;EM&gt;build/recipes/images/custom&lt;/EM&gt; as &lt;EM&gt;my_image.bb&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then using &lt;EM&gt;bitbake linux-imx -c menuconfig &lt;/EM&gt;I modified kernel configuration, again added some modules and removed some others.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I try &lt;EM&gt;bitbake my_image&lt;/EM&gt;, it gives me a bunch of errors as &lt;EM&gt;kernel-module-XXX not found in the base feeds&lt;/EM&gt;. Removing them from image recipe and adding other modules by hand will take a lot of time. Is there an easy way to update my &lt;EM&gt;my_image.bb&lt;/EM&gt; file so that it contains kernel-modules in my kernel config file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Durmuş&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 10:31:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Update-kernel-modules-in-image-recipe/m-p/489390#M78452</guid>
      <dc:creator>durmus</dc:creator>
      <dc:date>2016-04-29T10:31:14Z</dc:date>
    </item>
    <item>
      <title>Re: Update kernel modules in image recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Update-kernel-modules-in-image-recipe/m-p/489391#M78453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Durmus,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m afraid I’m not aware or any easy way to update the kernel modules contained in on your custom image to that they match the kernel config file. I’m not sure if working on a kernel configuration based on the current kernel of the image is an option but either way it will be a bit time consuming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 21:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Update-kernel-modules-in-image-recipe/m-p/489391#M78453</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-05-03T21:23:51Z</dc:date>
    </item>
  </channel>
</rss>