<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6UL burn eFuses from JTAG in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488791#M78304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You may try to download U-boot via JTAG and use it to burn the fuse.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Feb 2016 03:37:15 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-02-05T03:37:15Z</dc:date>
    <item>
      <title>IMX6UL burn eFuses from JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488790#M78303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with MCIMX6UL-EVK and i want to burn an eFuse, &lt;SPAN lang="en"&gt;specifically "UART Serial Download" which is 0x470[4].&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I connect with the board via JTAG and i am able to modify other registers however i can´t modify this eFuse.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Anybody knows if this is posible with JTAG? or may i do something before modifying the eFuse?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;We can't load any zimage or app because we can't make USB work, due to some issues we have with UART. The target of burning this eFuse is to disable uart detection so the USB is the first option in serial downloader mode. &lt;/SPAN&gt;&lt;SPAN lang="en"&gt;Then, i belive the PC will detect the board as HID unit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Please any help will be apreciated. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Thanks and best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 11:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488790#M78303</guid>
      <dc:creator>alubeiro</dc:creator>
      <dc:date>2016-02-04T11:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL burn eFuses from JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488791#M78304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You may try to download U-boot via JTAG and use it to burn the fuse.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 03:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488791#M78304</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-05T03:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL burn eFuses from JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488792#M78305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The u-boot files we got, are the ones that are into Mfgtool and they are ".imx" data files. Our JTAG "J-Link base" from Segger supports .mot, .srec, .s19, .s, .hex, .bin data files, so how can we do this?&lt;/P&gt;&lt;P&gt;I know that .imx data file includes a IVT header for the boot ROM to identify the u-boot's location &amp;amp; function etc...so i wonder how to load one of the above data files format.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then once the u-boot is downloaded, how can an e-fuse be burned?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are new in linux and therefore we are having a hard time making it works, so please be patient and don't spare details&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 08:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488792#M78305</guid>
      <dc:creator>alubeiro</dc:creator>
      <dc:date>2016-02-05T08:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL burn eFuses from JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488793#M78306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt; You may load and run the U-boot.imx as binary file, using information &lt;/P&gt;&lt;P&gt;of Table 8-26 (IVT Format) of the i.MX6UL RM. IVT is located in the beginning&lt;/P&gt;&lt;P&gt;of the file. &lt;BR /&gt;boot data (Absolute address of the Boot Data) - address to load &lt;/P&gt;&lt;P&gt;entry&amp;nbsp; (Absolute address of the first instruction to execute from the image) - start / run address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;Program the fuse values using the “fuse” command, available in i.MX U-Boot.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U_boot&amp;gt; fuse prog &amp;lt;bank&amp;gt; &amp;lt;word&amp;gt; &amp;lt;value&amp;gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt; The &amp;lt;bank&amp;gt; and &amp;lt;word&amp;gt; values are sourced from the Fuse Map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Feb 2016 08:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-burn-eFuses-from-JTAG/m-p/488793#M78306</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-09T08:05:25Z</dc:date>
    </item>
  </channel>
</rss>