<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDual Parallel Camera, I.MX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Dual-Parallel-Camera-I-MX6/m-p/488752#M78293</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to recieve 2ch, &lt;A href="mailto:720p@30fps"&gt;720p@30fps&lt;/A&gt;, BT.656, 4:2:2 format, 54MHz, each CSI port of I.MX6DUAL?&lt;/P&gt;&lt;P&gt;I think it can because there are two IPU units.&lt;/P&gt;&lt;P&gt;what do you think, experts?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32831i10DE61F4E65A1097/image-size/large?v=v2&amp;amp;px=999" title="v.jpg" alt="v.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Dec 2015 05:43:57 GMT</pubDate>
    <dc:creator>JHY</dc:creator>
    <dc:date>2015-12-17T05:43:57Z</dc:date>
    <item>
      <title>Dual Parallel Camera, I.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-Parallel-Camera-I-MX6/m-p/488752#M78293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to recieve 2ch, &lt;A href="mailto:720p@30fps"&gt;720p@30fps&lt;/A&gt;, BT.656, 4:2:2 format, 54MHz, each CSI port of I.MX6DUAL?&lt;/P&gt;&lt;P&gt;I think it can because there are two IPU units.&lt;/P&gt;&lt;P&gt;what do you think, experts?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32831i10DE61F4E65A1097/image-size/large?v=v2&amp;amp;px=999" title="v.jpg" alt="v.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 05:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-Parallel-Camera-I-MX6/m-p/488752#M78293</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-12-17T05:43:57Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Parallel Camera, I.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-Parallel-Camera-I-MX6/m-p/488753#M78294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Basically up to three cameras may be connected to the i.MX6 D/Q. &lt;/P&gt;&lt;P&gt;Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.&lt;/P&gt;&lt;P&gt;&amp;nbsp; According to section 9.2.1.1 (Camera Ports) :&lt;/P&gt;&lt;P&gt;"The input rate supported by the camera port is as follows:&lt;/P&gt;&lt;P&gt;• Peak: up to 240 MHz (values/sec)&lt;/P&gt;&lt;P&gt;• Average (assuming 35% blanking overhead), for YUV 4:2:2&lt;/P&gt;&lt;P&gt;• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps&lt;/P&gt;&lt;P&gt;• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 06:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-Parallel-Camera-I-MX6/m-p/488753#M78294</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-12-17T06:02:17Z</dc:date>
    </item>
  </channel>
</rss>