<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GUI on the fsl-image-gui build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GUI-on-the-fsl-image-gui-build/m-p/488375#M78230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FB backend is no GUI.&lt;/P&gt;&lt;P&gt;X11 backend will have a GUI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Dec 2015 08:50:16 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2015-12-17T08:50:16Z</dc:date>
    <item>
      <title>GUI on the fsl-image-gui build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GUI-on-the-fsl-image-gui-build/m-p/488374#M78229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've built the "fsl-image-gui" with a framebuffer back end for my SABRE Quad board and when I booted it up I saw a "Yocto project" boot bar, and then after the kernel booted it was replaced by a static image of a serial console. Basically a black screen that says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please wait: booting...&lt;/P&gt;&lt;P&gt;Poky (Yocto Project Reference Distro) 1.6.2 imx6qsabresd /dev/tty1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imxq6sabresd login:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not a true reflection of the serial console, as if I'm connected to minicom at the time, I can interact with the serial prompt but what I do is not mirrored over the HDMI, the HDMI always just shows the same static serial prompt login screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something I'm supposed to do to swap that login image for the actual GUI, which I assume is present on a "fsl-image-gui" build.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 14:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GUI-on-the-fsl-image-gui-build/m-p/488374#M78229</guid>
      <dc:creator>michaelworster</dc:creator>
      <dc:date>2015-12-16T14:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: GUI on the fsl-image-gui build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GUI-on-the-fsl-image-gui-build/m-p/488375#M78230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FB backend is no GUI.&lt;/P&gt;&lt;P&gt;X11 backend will have a GUI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 08:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GUI-on-the-fsl-image-gui-build/m-p/488375#M78230</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2015-12-17T08:50:16Z</dc:date>
    </item>
  </channel>
</rss>