<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx.6 boot from eMMC (eMMC version )</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-boot-from-eMMC-eMMC-version/m-p/487644#M78109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raviv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes possible, boot ROM will fall back to the eMMC4.4 standard &lt;/P&gt;&lt;P&gt;when a eMMC 5.0, 5.1 capable device is detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Dec 2015 01:51:35 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-17T01:51:35Z</dc:date>
    <item>
      <title>imx.6 boot from eMMC (eMMC version )</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-boot-from-eMMC-eMMC-version/m-p/487643#M78108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've noticed that the imx.6 can boot from eMMC 4.4 or lower.&lt;/P&gt;&lt;P&gt;would it be possible to boot a custom board from eMMC 5.0 or 5.1 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Raviv&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 15:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-boot-from-eMMC-eMMC-version/m-p/487643#M78108</guid>
      <dc:creator>ravivhaim</dc:creator>
      <dc:date>2015-12-16T15:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: imx.6 boot from eMMC (eMMC version )</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-boot-from-eMMC-eMMC-version/m-p/487644#M78109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raviv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes possible, boot ROM will fall back to the eMMC4.4 standard &lt;/P&gt;&lt;P&gt;when a eMMC 5.0, 5.1 capable device is detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 01:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-boot-from-eMMC-eMMC-version/m-p/487644#M78109</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-17T01:51:35Z</dc:date>
    </item>
  </channel>
</rss>