<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How should I make IMX53 processor run at full speed. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-make-IMX53-processor-run-at-full-speed/m-p/181642#M7810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you say SDIO device, do you mean SD card? SD cards can go up to 52MHz in speed, and 4-bit wide data transfer, so their performance will be limited (if you record a lot of data SD cards with higher speed class might help a little).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more speed, you'll need to look into using NAND, eMMC or SATA/SSD for storage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cpufreq is one of the tools that can be used to change CPU frequency on the fly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Nov 2012 07:21:35 GMT</pubDate>
    <dc:creator>VladanJovanovic</dc:creator>
    <dc:date>2012-11-23T07:21:35Z</dc:date>
    <item>
      <title>How should I make IMX53 processor run at full speed.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-make-IMX53-processor-run-at-full-speed/m-p/181641#M7809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a application, which runs very slow on IMX53 ubuntu 10.04. To meet my requirements I should run processor at high speed, so that it processes my SDIO device faster. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should I do to make processor run at very speed? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm already running the SDIO at higher clock speed (50MHz), but still that is not sufficient for me to process. Currently IMX processor is running at 300MHz, So I thought of increasing this processing speed by running processor at higher speed. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me in running the SDIO device at higher speed to achieve desired result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Swaraj&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2012 14:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-should-I-make-IMX53-processor-run-at-full-speed/m-p/181641#M7809</guid>
      <dc:creator>swaraj</dc:creator>
      <dc:date>2012-11-20T14:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: How should I make IMX53 processor run at full speed.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-make-IMX53-processor-run-at-full-speed/m-p/181642#M7810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you say SDIO device, do you mean SD card? SD cards can go up to 52MHz in speed, and 4-bit wide data transfer, so their performance will be limited (if you record a lot of data SD cards with higher speed class might help a little).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more speed, you'll need to look into using NAND, eMMC or SATA/SSD for storage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cpufreq is one of the tools that can be used to change CPU frequency on the fly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2012 07:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-should-I-make-IMX53-processor-run-at-full-speed/m-p/181642#M7810</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2012-11-23T07:21:35Z</dc:date>
    </item>
  </channel>
</rss>