<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: 4GB DDR3 Support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487600#M78084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suhas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Last year for testing purposes we equipped some few of our own i.MX6Q-based boards with 4pcs 8 GBit (512M16) DDR3 RAM-Chips from Intelligent Memory in 64-bit bus-configuration, i.e. all 4 chips connected to a single chip-select. Although we were not able to perform elaborate tests due to mechanical problems with the chips on our boards -- the 8 GBit chips from IM are slightly larger than all other DDR3 chips we equipped so far and unfortunately collided with some filter capacitors placed too close to the RAM-chips on the boards -- we were able to get two of the test-boards to (partially) functioning state, execute some few runtime-tests, and access the 3.75 GByte of memory mapped to the CPU-address space in such a configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, yes: 4 GByte RAM connected to a single chip-select of an i.MX6Q do work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While we haven't done any tests with the 8 GBit Micron type K you're asking for, we're using the 2 GBit and 4 GBit versions of these RAM-types without any problems in both DDR3-1066G amd DDR3-800E configurations and RAM-chips specified for higher clock-rates can be used at these clock-rates without any issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I know, the i.MX6 SoCs do not support any DDR3 clock-rates faster than 533 MHz (DDR3-1066).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Feb 2016 09:59:54 GMT</pubDate>
    <dc:creator>MOW</dc:creator>
    <dc:date>2016-02-11T09:59:54Z</dc:date>
    <item>
      <title>4GB DDR3 Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487599#M78083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: calibri, verdana, arial, sans-serif;"&gt;Hi Folks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: calibri, verdana, arial, sans-serif;"&gt;I have two queries to address:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-family: calibri, verdana, arial, sans-serif;"&gt;Planing to use single rank 4GB DDR3 (1GB Device x 4) using single Chip Select (CS0) in one of our design. Please let us know whether i.MX6Q supports such memory organisation that is 4GB on single Chip select.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-family: calibri, verdana, arial, sans-serif;"&gt;Pretty sure that i/MX6Q works fine with 533MHz DDR clock frequency. I have ambiguity in interfacing 800MHz DDR3 memory device with i.MX6. To be specific, whether &lt;STRONG&gt;MT41K512M16HA-125 IT&lt;/STRONG&gt; micron device can be used in above mentioned memory organization.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: calibri, verdana, arial, sans-serif;"&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: calibri, verdana, arial, sans-serif;"&gt;Suhas D K&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 13:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487599#M78083</guid>
      <dc:creator>suhasdk</dc:creator>
      <dc:date>2016-02-04T13:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: 4GB DDR3 Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487600#M78084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suhas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Last year for testing purposes we equipped some few of our own i.MX6Q-based boards with 4pcs 8 GBit (512M16) DDR3 RAM-Chips from Intelligent Memory in 64-bit bus-configuration, i.e. all 4 chips connected to a single chip-select. Although we were not able to perform elaborate tests due to mechanical problems with the chips on our boards -- the 8 GBit chips from IM are slightly larger than all other DDR3 chips we equipped so far and unfortunately collided with some filter capacitors placed too close to the RAM-chips on the boards -- we were able to get two of the test-boards to (partially) functioning state, execute some few runtime-tests, and access the 3.75 GByte of memory mapped to the CPU-address space in such a configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, yes: 4 GByte RAM connected to a single chip-select of an i.MX6Q do work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While we haven't done any tests with the 8 GBit Micron type K you're asking for, we're using the 2 GBit and 4 GBit versions of these RAM-types without any problems in both DDR3-1066G amd DDR3-800E configurations and RAM-chips specified for higher clock-rates can be used at these clock-rates without any issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I know, the i.MX6 SoCs do not support any DDR3 clock-rates faster than 533 MHz (DDR3-1066).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 09:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487600#M78084</guid>
      <dc:creator>MOW</dc:creator>
      <dc:date>2016-02-11T09:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: 4GB DDR3 Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487601#M78085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marc -&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the &amp;nbsp;i.MX6 docs are unclear on this point (4GB on single CS), can you comment on the&amp;nbsp;MMDC register changes &amp;nbsp;that were required moving to 4GB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Phil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 17:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4GB-DDR3-Support/m-p/487601#M78085</guid>
      <dc:creator>flournoy</dc:creator>
      <dc:date>2017-03-28T17:59:14Z</dc:date>
    </item>
  </channel>
</rss>