<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX51 buzzer driver using IO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181623#M7806</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The driver only allows to set the pulse width not frequency (fixed on initialization) using brightness. How do I change the PWM frequency?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Nov 2011 05:45:44 GMT</pubDate>
    <dc:creator>alsaleem</dc:creator>
    <dc:date>2011-11-02T05:45:44Z</dc:date>
    <item>
      <title>i.MX51 buzzer driver using IO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181621#M7804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there a way to output a variable frequency signal (audio range, 200-4K) square wave from i.MX51 to drive an external buzzer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Oct 2011 23:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181621#M7804</guid>
      <dc:creator>alsaleem</dc:creator>
      <dc:date>2011-10-30T23:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX51 buzzer driver using IO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181622#M7805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;PWM was&amp;nbsp;recommended for this case. It is more accurate and need less arm core's involvement.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2011 05:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181622#M7805</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2011-11-02T05:26:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX51 buzzer driver using IO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181623#M7806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The driver only allows to set the pulse width not frequency (fixed on initialization) using brightness. How do I change the PWM frequency?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2011 05:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181623#M7806</guid>
      <dc:creator>alsaleem</dc:creator>
      <dc:date>2011-11-02T05:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX51 buzzer driver using IO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181624#M7807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;That's right, PWM is designed for brightness tuning, but it can also be used&amp;nbsp;flexibly. &amp;nbsp;Actually, the&amp;nbsp;PERIOD can be programmed (see Chapter&amp;nbsp;47.2.2.5, mx51RM for the detail.) &amp;nbsp;and &amp;nbsp;the frequency is much accurate that GPIO way. Anyway, if the accuracy&amp;nbsp; is not important, such as for a buzzer, the GPIO method should be OK.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2011 07:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-buzzer-driver-using-IO/m-p/181624#M7807</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2011-11-02T07:49:39Z</dc:date>
    </item>
  </channel>
</rss>