<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTouch control?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Touch-control/m-p/149507#M780</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi every one.&lt;/P&gt;&lt;P&gt;I have some trouble about the touch lcd.&lt;/P&gt;&lt;P&gt;The freescale's lcd is seiko&amp;nbsp;43WVFIG. That's work good.&lt;/P&gt;&lt;P&gt;My lcd is ampire AM-800480L with the same resolution but the size is bigger, that's display well.&lt;/P&gt;&lt;P&gt;Both of them have the touch panel with 4 line connect to imx53.&lt;/P&gt;&lt;P&gt;I use the seiko driver to control ampire.I can touch the panel of ampire but the imx not get right position ( error about 2-3mm, I just measure by my eye).&lt;/P&gt;&lt;P&gt;I don't familliar with os system, that's I can't understand how it works.&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;P&gt;- I want to debug the position when I touch to the panel of LCD.&lt;/P&gt;&lt;P&gt;What file I need to modify to printf the x-y position to visual 2008 (in debug mode)?&lt;/P&gt;&lt;P&gt;After that I want to modify to make imx53 understand right position.&lt;/P&gt;&lt;P&gt;- If possible, can you explain what OS system work? Does it like the microcontroller work in file main.c and if interrupt happen that jump to interrupt function?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2012 04:44:21 GMT</pubDate>
    <dc:creator>HaiDangSon</dc:creator>
    <dc:date>2012-03-29T04:44:21Z</dc:date>
    <item>
      <title>Touch control?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-control/m-p/149507#M780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi every one.&lt;/P&gt;&lt;P&gt;I have some trouble about the touch lcd.&lt;/P&gt;&lt;P&gt;The freescale's lcd is seiko&amp;nbsp;43WVFIG. That's work good.&lt;/P&gt;&lt;P&gt;My lcd is ampire AM-800480L with the same resolution but the size is bigger, that's display well.&lt;/P&gt;&lt;P&gt;Both of them have the touch panel with 4 line connect to imx53.&lt;/P&gt;&lt;P&gt;I use the seiko driver to control ampire.I can touch the panel of ampire but the imx not get right position ( error about 2-3mm, I just measure by my eye).&lt;/P&gt;&lt;P&gt;I don't familliar with os system, that's I can't understand how it works.&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;P&gt;- I want to debug the position when I touch to the panel of LCD.&lt;/P&gt;&lt;P&gt;What file I need to modify to printf the x-y position to visual 2008 (in debug mode)?&lt;/P&gt;&lt;P&gt;After that I want to modify to make imx53 understand right position.&lt;/P&gt;&lt;P&gt;- If possible, can you explain what OS system work? Does it like the microcontroller work in file main.c and if interrupt happen that jump to interrupt function?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2012 04:44:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-control/m-p/149507#M780</guid>
      <dc:creator>HaiDangSon</dc:creator>
      <dc:date>2012-03-29T04:44:21Z</dc:date>
    </item>
  </channel>
</rss>