<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMx53 VPU&amp;IPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMx53-VPU-IPU/m-p/487139#M77990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepanraj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for vpu firmware please refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;Table 18-3. VPU firmware Files. It works with vpu codecs on below links&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board Support Packages (8)&lt;/P&gt;&lt;P&gt;Linux 2.6.35 Source Code Files and documentation 11.09&lt;/P&gt;&lt;P&gt;"Linux Multimedia Codecs Documentation and Sources 11.09 for i.MX53 for the&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Codecs and other Algorithms (1)&lt;/P&gt;&lt;P&gt;Quick Start boards.Updated with the Linux 11.09 patch release and the 2.0.5 Open Max files. (REV 2011.09.03)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IPU drivers are described in Chapter 10 Image Processing Unit (IPU) Drivers,&lt;/P&gt;&lt;P&gt;regarding dependencies one can check attached Release Notes&lt;/P&gt;&lt;P&gt;Table 1-1,Table 1-2 show used kernel,toolchain versions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Feb 2016 07:53:12 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-02-04T07:53:12Z</dc:date>
    <item>
      <title>iMx53 VPU&amp;IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx53-VPU-IPU/m-p/487138#M77989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ours is IMx53 processor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any Binaries/Firmware dependency to be loaded for VPU and IPU drivers on imx53.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If Binaries or Firmware is required Please share the link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 07:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx53-VPU-IPU/m-p/487138#M77989</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2016-02-04T07:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: iMx53 VPU&amp;IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx53-VPU-IPU/m-p/487139#M77990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepanraj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for vpu firmware please refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;Table 18-3. VPU firmware Files. It works with vpu codecs on below links&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board Support Packages (8)&lt;/P&gt;&lt;P&gt;Linux 2.6.35 Source Code Files and documentation 11.09&lt;/P&gt;&lt;P&gt;"Linux Multimedia Codecs Documentation and Sources 11.09 for i.MX53 for the&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Codecs and other Algorithms (1)&lt;/P&gt;&lt;P&gt;Quick Start boards.Updated with the Linux 11.09 patch release and the 2.0.5 Open Max files. (REV 2011.09.03)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IPU drivers are described in Chapter 10 Image Processing Unit (IPU) Drivers,&lt;/P&gt;&lt;P&gt;regarding dependencies one can check attached Release Notes&lt;/P&gt;&lt;P&gt;Table 1-1,Table 1-2 show used kernel,toolchain versions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 07:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx53-VPU-IPU/m-p/487139#M77990</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-02-04T07:53:12Z</dc:date>
    </item>
  </channel>
</rss>