<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic opengl transparent type frame  buffer config  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/opengl-transparent-type-frame-buffer-config/m-p/486888#M77930</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to create Opengl surface with below attributes from eglchooseconfig:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_TYPE=EGL_NONE&lt;/P&gt;&lt;P&gt;EGL_RED_SIZE/EGL_GREEN_SIZE/EGL_BLUE_SIZE/EGL_ALPHA_SIZE=8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i did eglchooseconfig i was able to retrieve a "config" for this combination using which i can create a surface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But for below combinations&amp;nbsp; I am not able retrieve any "config" and it fails &lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_TYPE=EGL_NONE&lt;/P&gt;&lt;P&gt;EGL_RED_SIZE/EGL_GREEN_SIZE/EGL_BLUE_SIZE/EGL_ALPHA_SIZE=8&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_RED_VALUE/EGL_TRANSPARENT_GREEN_VALUE/EGL_TRANSPARENT_BLUE_VALUE=8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_TYPE=EGL_TRANSPARENT_RGB&lt;/P&gt;&lt;P&gt;EGL_RED_SIZE/EGL_GREEN_SIZE/EGL_BLUE_SIZE/EGL_ALPHA_SIZE=8&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_RED_VALUE/EGL_TRANSPARENT_GREEN_VALUE/EGL_TRANSPARENT_BLUE_VALUE=8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i see that if framebuffer can support transparent we can use these combinations. I think imx6 shall support it since i have these macros in egl.h. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am i missing something here......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Feb 2016 11:55:29 GMT</pubDate>
    <dc:creator>satyanarayanamu</dc:creator>
    <dc:date>2016-02-04T11:55:29Z</dc:date>
    <item>
      <title>opengl transparent type frame  buffer config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/opengl-transparent-type-frame-buffer-config/m-p/486888#M77930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to create Opengl surface with below attributes from eglchooseconfig:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_TYPE=EGL_NONE&lt;/P&gt;&lt;P&gt;EGL_RED_SIZE/EGL_GREEN_SIZE/EGL_BLUE_SIZE/EGL_ALPHA_SIZE=8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i did eglchooseconfig i was able to retrieve a "config" for this combination using which i can create a surface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But for below combinations&amp;nbsp; I am not able retrieve any "config" and it fails &lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_TYPE=EGL_NONE&lt;/P&gt;&lt;P&gt;EGL_RED_SIZE/EGL_GREEN_SIZE/EGL_BLUE_SIZE/EGL_ALPHA_SIZE=8&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_RED_VALUE/EGL_TRANSPARENT_GREEN_VALUE/EGL_TRANSPARENT_BLUE_VALUE=8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_TYPE=EGL_TRANSPARENT_RGB&lt;/P&gt;&lt;P&gt;EGL_RED_SIZE/EGL_GREEN_SIZE/EGL_BLUE_SIZE/EGL_ALPHA_SIZE=8&lt;/P&gt;&lt;P&gt;EGL_TRANSPARENT_RED_VALUE/EGL_TRANSPARENT_GREEN_VALUE/EGL_TRANSPARENT_BLUE_VALUE=8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i see that if framebuffer can support transparent we can use these combinations. I think imx6 shall support it since i have these macros in egl.h. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am i missing something here......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 11:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/opengl-transparent-type-frame-buffer-config/m-p/486888#M77930</guid>
      <dc:creator>satyanarayanamu</dc:creator>
      <dc:date>2016-02-04T11:55:29Z</dc:date>
    </item>
  </channel>
</rss>