<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx6 Audio Clock source form clk2_p/n in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486211#M77789</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for reply,&lt;/P&gt;&lt;P&gt;i meas i follow the SABRE AI CPU Card schematic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;use 24.576 oscillator&amp;nbsp; with a converter to CLK2_P/N .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then we want to ouput i2s signal as w5/BCLK;V6/DOUT/;U7/LRCLK,&lt;/P&gt;&lt;P&gt;so how can we to configuration the code to do this function?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Apr 2016 03:57:45 GMT</pubDate>
    <dc:creator>darrenwang</dc:creator>
    <dc:date>2016-04-29T03:57:45Z</dc:date>
    <item>
      <title>i.mx6 Audio Clock source form clk2_p/n</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486209#M77787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can we get the Audio Clk 24.576 MHZ from i.mx6 CLK2_P/CLK2_N? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We want to output the i2s signal for audio dac, but we use an oscillator at i.mx6 pin D5 and pin D5.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 06:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486209#M77787</guid>
      <dc:creator>darrenwang</dc:creator>
      <dc:date>2016-04-28T06:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Audio Clock source form clk2_p/n</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486210#M77788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First, please note that CLK2_P and CLK2_N are the differential LVDS signals, not a regular logic High/Low signals. Most likely, your audio codec IC does not support the LVDS clock input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Second, there seems to be no appropriate clock source inside i.MX6 processor (if using regular 24MHz crystal as the clock reference) to generate 24.576MHz frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, most likely, the answer is: no, it is not possible to use the CLK2_P and CLK2_N pins to output the 24.576MHz clock to an external audio codec.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 09:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486210#M77788</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-04-28T09:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Audio Clock source form clk2_p/n</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486211#M77789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for reply,&lt;/P&gt;&lt;P&gt;i meas i follow the SABRE AI CPU Card schematic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;use 24.576 oscillator&amp;nbsp; with a converter to CLK2_P/N .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then we want to ouput i2s signal as w5/BCLK;V6/DOUT/;U7/LRCLK,&lt;/P&gt;&lt;P&gt;so how can we to configuration the code to do this function?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 03:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Audio-Clock-source-form-clk2-p-n/m-p/486211#M77789</guid>
      <dc:creator>darrenwang</dc:creator>
      <dc:date>2016-04-29T03:57:45Z</dc:date>
    </item>
  </channel>
</rss>