<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: HAB - fast authentication or not?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HAB-fast-authentication-or-not/m-p/485281#M77485</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexey&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fast Authentication supported by HAB 4.1.2 and later (only MX6SX, MX6UL and MX7D)&lt;/P&gt;&lt;P&gt;reduces the number of keys required to sign the image from two to one and&lt;/P&gt;&lt;P&gt;minimum number of RSA operations from four to two (25ms to 12.5ms typically),&lt;/P&gt;&lt;P&gt;examples can be found on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="275249" data-objecttype="102" href="https://community.freescale.com/docs/DOC-275249"&gt;https://community.freescale.com/docs/DOC-275249&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2016 01:33:33 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-01-13T01:33:33Z</dc:date>
    <item>
      <title>HAB - fast authentication or not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-fast-authentication-or-not/m-p/485280#M77484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello dear all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to bring up HAB authentication for Windows Embedded Compact bootloader (eboot).&lt;/P&gt;&lt;P&gt;Just soved the issue with call HAB ROM to check for its status and events so now I am ready to proceed for the next stage.&lt;/P&gt;&lt;P&gt;So I installed CST, read the docs and started generating keys but I am not sure whether I need/can use fast authentication or not.&lt;/P&gt;&lt;P&gt;My goal is to make iMX chip only load signed EBOOT, remaining security checks are done (implemented) by using Microsoft authentication security libraries.&lt;/P&gt;&lt;P&gt;So I am not going to authenticate anythyng else with iMX6, just EBOOT and I really want it to be done in the simplest possible way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use fast authentication for such a case or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read that it is supported not in all iMX6 chips so assuming I need to use various iMX6 chips in various products but want keep the same&lt;/P&gt;&lt;P&gt;executable running on all platforms I can't use fast path, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, if I use normal authentication and get all those keys generated (IMG and CSF etc.) can it prevent me from just checking my EBOOT with iMX6&lt;/P&gt;&lt;P&gt;and leaving any other authentication done by using MS libraries?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any other suggestions would be nice as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and sorry for (possibly) bad english.&lt;/P&gt;&lt;P&gt;Alexey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 17:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-fast-authentication-or-not/m-p/485280#M77484</guid>
      <dc:creator>AlexeyT</dc:creator>
      <dc:date>2016-01-12T17:35:45Z</dc:date>
    </item>
    <item>
      <title>Re: HAB - fast authentication or not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-fast-authentication-or-not/m-p/485281#M77485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexey&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fast Authentication supported by HAB 4.1.2 and later (only MX6SX, MX6UL and MX7D)&lt;/P&gt;&lt;P&gt;reduces the number of keys required to sign the image from two to one and&lt;/P&gt;&lt;P&gt;minimum number of RSA operations from four to two (25ms to 12.5ms typically),&lt;/P&gt;&lt;P&gt;examples can be found on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="275249" data-objecttype="102" href="https://community.freescale.com/docs/DOC-275249"&gt;https://community.freescale.com/docs/DOC-275249&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 01:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-fast-authentication-or-not/m-p/485281#M77485</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-13T01:33:33Z</dc:date>
    </item>
  </channel>
</rss>