<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: adb over network through sdcard booting (Android) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/adb-over-network-through-sdcard-booting-Android/m-p/485191#M77475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure that the network is configured correctly in SD-card case.&lt;/P&gt;&lt;P&gt;I mean please try to perform some other TCP connection between the board and host machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 May 2016 03:09:27 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-05-24T03:09:27Z</dc:date>
    <item>
      <title>adb over network through sdcard booting (Android)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-over-network-through-sdcard-booting-Android/m-p/485190#M77474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I enabled one property &lt;SPAN style="color: #3334ca;"&gt;service.adb.tcp.port 5555&lt;/SPAN&gt; for adb over network. Its working fine after typing command &lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #7ed529;"&gt;adb connect &amp;lt;ip-address&amp;gt;&lt;/SPAN&gt; in emmc booting for android 5.0.2 and its not working after typing command&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #7ed529;"&gt;adb connect &amp;lt;ip-address&amp;gt; &lt;/SPAN&gt;in sdcard booting for android 5.0.2 with same device but difference is only booting mode. Please help me any extra property i need to add for adb over network through sdcard booting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 09:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-over-network-through-sdcard-booting-Android/m-p/485190#M77474</guid>
      <dc:creator>chandrasekharma</dc:creator>
      <dc:date>2016-05-19T09:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: adb over network through sdcard booting (Android)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-over-network-through-sdcard-booting-Android/m-p/485191#M77475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure that the network is configured correctly in SD-card case.&lt;/P&gt;&lt;P&gt;I mean please try to perform some other TCP connection between the board and host machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 May 2016 03:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-over-network-through-sdcard-booting-Android/m-p/485191#M77475</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-05-24T03:09:27Z</dc:date>
    </item>
  </channel>
</rss>