<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR Calibration on i.MX53 - REVISTED in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484759#M77395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can help you with this. I've done a lot of work with the stress tester.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Read my posts in this thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/355451"&gt;i.MX536: DDR Stress test failed when the temperature of DDR increase upper to 80 degree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do we send private messages in this "community"? I can't find how to do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right. I can't send you a message because you aren't my "friend" and you're not "following" me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if you "follow" me I'll be able to send you a message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 03 Jan 2016 02:10:41 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2016-01-03T02:10:41Z</dc:date>
    <item>
      <title>DDR Calibration on i.MX53 - REVISTED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484757#M77393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;This posting is regarding a previous post:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/418938#418938"&gt;https://community.freescale.com/message/418938#418938&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d;"&gt;That post is relevant to my problem, but does not have the complete answer. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d;"&gt;It says that we have to make a program that runs the calibration routines (calibration.c) in IRAM.&amp;nbsp; It also points to processor expert for Imx53, which does not seem to work as per the post. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d;"&gt;The steps are not very clear about making the program and running it in IRAM. I will appreciate, if you could offer a little more guidance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know, there is StressTester.exe which we use to do ddr stress test. However, I need an application (or source) to run the calibration and get the proper values for some production boards in the field that are acting strangly. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some routines I got from Application Note (AN4466), but I am not sure how can I run those routines. These routines are supposed to be run in CPU ram, so obviously there has to be an application on PC that connects to IMX53 using USB and run these routines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help in advance,&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 20:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484757#M77393</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2015-12-15T20:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Calibration on i.MX53 - REVISTED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484758#M77394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use jtag:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94841"&gt;i.MX53 Memory Calibration Script (AN4466)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;or use attached example (add own codes) with ATK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 01:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484758#M77394</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-16T01:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Calibration on i.MX53 - REVISTED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484759#M77395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can help you with this. I've done a lot of work with the stress tester.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Read my posts in this thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/355451"&gt;i.MX536: DDR Stress test failed when the temperature of DDR increase upper to 80 degree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do we send private messages in this "community"? I can't find how to do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right. I can't send you a message because you aren't my "friend" and you're not "following" me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if you "follow" me I'll be able to send you a message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 02:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484759#M77395</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2016-01-03T02:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Calibration on i.MX53 - REVISTED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484760#M77396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Like I said, if you FOLLOW me I'll be able to help - by sending a working version of the Stress Test you can load over Ethernet and run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've "followed" you, so you can send me a message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 01:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Calibration-on-i-MX53-REVISTED/m-p/484760#M77396</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2016-01-29T01:18:03Z</dc:date>
    </item>
  </channel>
</rss>