<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Microcode SW error detected.  Restarting 0x2000000.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181311#M7734</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tonie, did Israel answer your question. If yes, please click Correct Answer button so that we can close the DI.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yixing,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2013 06:12:02 GMT</pubDate>
    <dc:creator>imxcommunitysco</dc:creator>
    <dc:date>2013-01-09T06:12:02Z</dc:date>
    <item>
      <title>Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181309#M7732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I am trying to port Intel Centrino-N 135 wifi module into iMx6q. (Android ICS version, code base is R13.4)&lt;/P&gt;&lt;P&gt;For figuring out what issues are I met, here are my procedures :&lt;/P&gt;&lt;P&gt;1. insmod cfg80211.ko&lt;/P&gt;&lt;P&gt;2. insmod mac80211.ko&lt;/P&gt;&lt;P&gt;3. insmod iwlan.ko debug=0x43ffff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Till now, those output messages are quite ok.&lt;/P&gt;&lt;P&gt;Then I started the wpa_supplicant, then those messages are coming :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;start wpa_supplicant&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_mac_start enter&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_prep_station Add STA to driver ID 15: ff:ff:ff:ff:ff:ff&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_prep_station Add STA to driver ID 14: ff:ff:ff:ff:ff:ff&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_prepare_card_hw iwl_prepare_card_hw enter&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_set_hw_ready hardware ready&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_init Init card's basic functions&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_init L1 Disabled; Enabling L0S&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_load_section INST uCode section being loaded...&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_load_section DATA uCode section being loaded...&lt;/P&gt;&lt;P&gt;ieee80211 phy0: I iwlagn_alive_fn Alive ucode status 0x00000001 revision 0x1 0x9&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlcore_verify_inst_sparse ucode inst image size is 139180&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_verify_ucode uCode is good in inst SRAM&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 0 on FIFO 3&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 1 on FIFO 2&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 2 on FIFO 1&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 3 on FIFO 0&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 4 on FIFO 0&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 5 on FIFO 4&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 6 on FIFO 2&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 7 on FIFO 5&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 8 on FIFO 4&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 9 on FIFO 7&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_send_cmd_sync Attempting to send sync command COEX_PRIORITY_TABLE_CMD&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_send_cmd_sync Setting HCMD_ACTIVE for command COEX_PRIORITY_TABLE_CMD&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_enqueue_hcmd Sending command COEX_PRIORITY_TABLE_CMD (#5a), seq: 0x0900, 72 bytes at 0[0]:9&lt;/P&gt;&lt;P&gt;ieee80211 phy0: I iwl_tx_cmd_complete Clearing HCMD_ACTIVE for command COEX_PRIORITY_TABLE_CMD&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Microcode SW error detected.&amp;nbsp; Restarting 0x2000000.&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Loaded firmware version: 18.168.6.1&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Start IWL Error Log Dump:&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Status: 0x00040224, count: 6&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x000019B4 | ADVANCED_SYSASSERT&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00014D38 | uPc&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00014D2A | branchlink1&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00014D2A | branchlink2&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x0000CDCE | interruptlink1&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000000 | interruptlink2&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x0000021F | data1&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000171 | data2&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000171 | line&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x004071C0 | beacon time&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x0002AE40 | tsf low&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000000 | tsf hi&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000000 | time gp1&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x0002AE44 | time gp2&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000000 | time gp3&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x754312A8 | uCode version&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00000120 | hw version&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x00C80300 | board version&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: 0x0900005A | hcmd&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: CSR values:&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: (2nd byte of CSR_INT_COALESCING is CSR_INT_PERIODIC_REG)&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_HW_IF_CONFIG_REG: 0X00c80300&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_INT_COALESCING: 0X0000ff40&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_INT: 0X10000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_INT_MASK: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_FH_INT_STATUS: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_GPIO_IN: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_RESET: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_GP_CNTRL: 0X080403c5&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_HW_REV: 0X00000120&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_EEPROM_REG: 0X45180ffd&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_EEPROM_GP: 0X90000801&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_OTP_GP_REG: 0X00030001&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_GIO_REG: 0X00080044&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_GP_UCODE_REG: 0X0000001e&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_GP_DRIVER_REG: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_UCODE_DRV_GP1: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_UCODE_DRV_GP2: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_LED_REG: 0X00000018&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_DRAM_INT_TBL_REG: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_GIO_CHICKEN_BITS: 0X29800200&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_ANA_PLL_CFG: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_HW_REV_WA_REG: 0X0001001a&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CSR_DBG_HPET_MEM_REG: 0Xffff0000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: FH register values:&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_RSCSR_CHNL0_STTS_WPTR_REG: 0X0279d100&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_RSCSR_CHNL0_RBDCB_BASE_REG: 0X0027e2d0&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_RSCSR_CHNL0_WPTR: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_MEM_RCSR_CHNL0_CONFIG_REG: 0X80819104&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_MEM_RSSR_SHARED_CTRL_REG: 0X000000fc&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_MEM_RSSR_RX_STATUS_REG: 0X07030000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_MEM_RSSR_RX_ENABLE_ERR_IRQ2DRV: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_TSSR_TX_STATUS_REG: 0X07ff0001&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FH_TSSR_TX_ERROR_REG: 0X00000000&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Start IWL Event Log Dump: display last 20 entries&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000026983:0x000000ff:1100&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000026984:0x000000ff:1100&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000026985:0x000000ff:1100&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000026985:0x000000ff:1100&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000026986:0x000000ff:1100&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174346:0x0900005a:0401&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174347:0x0900005a:1512&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174457:0x00000003:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174457:0x00000003:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174458:0x00000000:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174460:0x00000004:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174461:0x00000003:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174464:0x00000001:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174464:0x00000000:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174465:0x00000001:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174466:0x00000001:1211&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000174466:0xcafe0001:1214&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000175229:0x0002ac7d:1110&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000175681:0x0000021f:1132&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: EVT_LOGT:0000175691:0x00000000:0125&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_send_cmd_sync Attempting to send sync command REPLY_PHY_CALIBRATION_CMD&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_send_cmd_sync Setting HCMD_ACTIVE for command REPLY_PHY_CALIBRATION_CMD&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_enqueue_hcmd Sending command REPLY_PHY_CALIBRATION_CMD (#b0), seq: 0x0901, 12 bytes at 1[1]:9&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Error sending REPLY_PHY_CALIBRATION_CMD: time out after 500ms.&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_send_cmd_sync Clearing HCMD_ACTIVE for command REPLY_PHY_CALIBRATION_CMD&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Error -110 iteration 0&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Could not complete ALIVE transition: -110&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_stop Stop card, put in low power state&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_stop_master stop master&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Failed to run INIT ucode: -110&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U __iwl_down iwlagn is going down&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_scan_cancel_timeout Scan cancel timeout&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_do_scan_abort Not performing scan to abort&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_clear_ucode_stations Clearing ucode stations in driver&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_clear_ucode_stations No active stations found to be cleared&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_stop Stop card, put in low power state&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_stop_master stop master&lt;/P&gt;&lt;P&gt;iwlagn 0000:01:00.0: Unable to initialize device.&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U __iwl_down iwlagn is going down&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_scan_cancel_timeout Scan cancel timeout&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_do_scan_abort Not performing scan to abort&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_clear_ucode_stations Clearing ucode stations in driver&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_clear_ucode_stations No active stations found to be cleared&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_stop Stop card, put in low power state&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwl_apm_stop_master stop master&lt;/P&gt;&lt;P&gt;ieee80211 phy0: Hardware restart was requested&lt;/P&gt;&lt;P&gt;ieee80211 phy0: U iwlagn_configure_filter Enter: changed: 0x0, total: 0x80000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@android:/system/lib/modules #&lt;/P&gt;&lt;P&gt;root@android:/system/lib/modules # logcat&lt;/P&gt;&lt;P&gt;--------- beginning of /dev/log/main&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): wpa_supplicant v0.8.x&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Add randomness: count=1 entropy=0&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): random: Added entropy from /data/misc/wifi/entropy.bin (own_pool_ready=2)&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): random: Trying to read entropy from /dev/random&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Get randomness: len=20 entropy=1&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): random: Updated entropy file /data/misc/wifi/entropy.bin (own_pool_ready=2)&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Initializing interface 'wlan0' conf '/system/etc/wifi/wpa_supplicant.conf' driver 'nl80211' ctrl_interface 'N/A' bridge 'N/A'&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Configuration file '/system/etc/wifi/wpa_supplicant.conf' -&amp;gt; '/system/etc/wifi/wpa_supplicant.conf'&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Reading configuration file '/system/etc/wifi/wpa_supplicant.conf'&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): update_config=1&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): ctrl_interface='DIR=/data/system/wpa_supplicant GROUP=wifi'&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): ap_scan=0&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Line: 8 - start of a new network block&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): key_mgmt: 0x4&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Priority group 0&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917):&amp;nbsp;&amp;nbsp;&amp;nbsp; id=0 ssid=''&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): nl80211: interface wlan0 in phy phy0&lt;/P&gt;&lt;P&gt;I/wpa_supplicant( 2917): rfkill: Cannot open RFKILL control device&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): nl80211: RFKILL status not available&lt;/P&gt;&lt;P&gt;E/wpa_supplicant( 2917): Could not set interface wlan0 flags: Connection timed out&lt;/P&gt;&lt;P&gt;E/wpa_supplicant( 2917): nl80211: Could not set interface 'wlan0' UP&lt;/P&gt;&lt;P&gt;E/wpa_supplicant( 2917): wlan0: Failed to initialize driver interface&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Failed to add interface wlan0&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): Get randomness: len=20 entropy=0&lt;/P&gt;&lt;P&gt;D/wpa_supplicant( 2917): random: Updated entropy file /data/misc/wifi/entropy.bin (own_pool_ready=2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone give me hint or suggestion ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tonie&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2012 14:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181309#M7732</guid>
      <dc:creator>toniehuang</dc:creator>
      <dc:date>2012-11-20T14:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181310#M7733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seem to be a problem with the physical layer. &lt;/P&gt;&lt;P&gt;Are you using a PCI express module? Or is USB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ask because similar errors also appear on Bluetooth layer when the buadrate, parity or link layer are not setup&lt;/P&gt;&lt;P&gt;properly to the ones stored in the chip firmware then it will start to generate timeouts and also frame errors.&lt;/P&gt;&lt;P&gt;Do you have that information for that wifi module?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Israel&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 22:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181310#M7733</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2013-01-04T22:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181311#M7734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tonie, did Israel answer your question. If yes, please click Correct Answer button so that we can close the DI.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yixing,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 06:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181311#M7734</guid>
      <dc:creator>imxcommunitysco</dc:creator>
      <dc:date>2013-01-09T06:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181312#M7735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Seem to be a problem with the physical layer.&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Are you using a PCI express module? Or is USB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;I ask because similar errors also appear on Bluetooth layer when the buadrate, parity or link layer are not setup&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;properly to the ones stored in the chip firmware then it will start to generate timeouts and also frame errors.&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Do you have that information for that wifi module?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Regards,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;-Israel&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;SPAN class="mce_paste_marker" style="font-style: inherit; font-family: inherit;"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 17:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181312#M7735</guid>
      <dc:creator>israelpz</dc:creator>
      <dc:date>2013-01-10T17:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181313#M7736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Israel,&lt;/P&gt;&lt;P&gt;Sorry for lately response.&lt;/P&gt;&lt;P&gt;What I used is PCI express modules.&lt;/P&gt;&lt;P&gt;And I didn't have any further information about that wifi module. (Intel doesn't release any doc to us)&lt;/P&gt;&lt;P&gt;All I have is those file from the opensource of Intel wifi module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tonie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2013 06:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181313#M7736</guid>
      <dc:creator>toniehuang</dc:creator>
      <dc:date>2013-01-14T06:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181314#M7737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tony,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at detail on the error dump i could say the following:&lt;/P&gt;&lt;P&gt;Even your are using a intel PCI express. Internally they use a CSR wifi ip.&lt;/P&gt;&lt;P&gt;The setup registers which could be configured at boot time on CSR chips are call PSKEYS like&lt;/P&gt;&lt;P&gt;"&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;CSR_HW_IF_CONFIG_REG&lt;/SPAN&gt;", "&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;CSR_UCODE_DRV_GP2&lt;/SPAN&gt;" , etc.&lt;/P&gt;&lt;P&gt;Those registers are documented in NDA technical document provided by CSR.&lt;/P&gt;&lt;P&gt;The problem here is somehow a binary with the PSKEYS is loaded but that cause a failure in&lt;/P&gt;&lt;P&gt;the communication with the CSR wifi module (that is very similar to a issue Bluetooth module).&lt;/P&gt;&lt;P&gt;The only way to solved it is not loading that binary(firmware bin) or ask intel to provide a tested/working firmware binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Israel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2013 15:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181314#M7737</guid>
      <dc:creator>israelpz</dc:creator>
      <dc:date>2013-01-14T15:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181315#M7738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Israel,&lt;/P&gt;&lt;P&gt;Thanks for your information.&lt;/P&gt;&lt;P&gt;I will try to follow your suggestion and tell if I have any result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tonie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2013 03:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181315#M7738</guid>
      <dc:creator>toniehuang</dc:creator>
      <dc:date>2013-01-18T03:08:44Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181316#M7739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm having the same issue using a pcie card with Intel 6235 on an i.mx6 board with kernel 3.0.35.&lt;/P&gt;&lt;P&gt;Have you been able to solve this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 08:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181316#M7739</guid>
      <dc:creator>mralmond</dc:creator>
      <dc:date>2014-02-18T08:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: Microcode SW error detected.  Restarting 0x2000000.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181317#M7740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I've fixed this issue by other way.&lt;/P&gt;&lt;P&gt;As we know that the driver for Intel wifi modules came from backports-3.xxxx... (or compat-wireless-xxxx)&lt;/P&gt;&lt;P&gt;What I did was :&lt;/P&gt;&lt;P&gt;I download many different version of intel wirelss driver and try to port into my board.&lt;/P&gt;&lt;P&gt;And I found one version of these can work without modifying may code in driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is just what I did and how I fix my issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 02:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Microcode-SW-error-detected-Restarting-0x2000000/m-p/181317#M7740</guid>
      <dc:creator>toniehuang</dc:creator>
      <dc:date>2014-10-24T02:07:46Z</dc:date>
    </item>
  </channel>
</rss>