<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: LCD Expansion Port not working with Sabre Android BSP Demo images</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484308#M77284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, confirming the same.&amp;nbsp; Neither the MCIMX28LCD or MCIMXHDMICARD worked with out-of-the-box Android images for the IMX6SX.&amp;nbsp;&amp;nbsp; Purchased the MCIMX-LVDS1 and this worked as expected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jul 2016 18:01:24 GMT</pubDate>
    <dc:creator>btjosh</dc:creator>
    <dc:date>2016-07-26T18:01:24Z</dc:date>
    <item>
      <title>LCD Expansion Port not working with Sabre Android BSP Demo images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484306#M77282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The iMX6 SoloX Sabre board LCD Expansion Port is not working with the default BSP images for Android.&lt;/P&gt;&lt;P&gt;Both MCIMX28LCD and MCIMXHDMICARD are not recognized when connected.&amp;nbsp; I do not have the LVDS based LCD display, so I am unable to test if video is working using that either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone comment how to configure the default Android Sabre BSP images to work with either of MCIMX28LCD or MCIMXHDMICARD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried many comments in the discussion forum here on configuring U-boot with specific bootargs, but nothing has worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 14:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484306#M77282</guid>
      <dc:creator>btjosh</dc:creator>
      <dc:date>2016-05-19T14:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: LCD Expansion Port not working with Sabre Android BSP Demo images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484307#M77283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;refer to the android relese note, mx6sx supports lvds only, but for linux, as I known can support hdmi (sii902x), if you need to support hdmi you should refere to the yocto bsp driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 06:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484307#M77283</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-05-25T06:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: LCD Expansion Port not working with Sabre Android BSP Demo images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484308#M77284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, confirming the same.&amp;nbsp; Neither the MCIMX28LCD or MCIMXHDMICARD worked with out-of-the-box Android images for the IMX6SX.&amp;nbsp;&amp;nbsp; Purchased the MCIMX-LVDS1 and this worked as expected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 18:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-Expansion-Port-not-working-with-Sabre-Android-BSP-Demo/m-p/484308#M77284</guid>
      <dc:creator>btjosh</dc:creator>
      <dc:date>2016-07-26T18:01:24Z</dc:date>
    </item>
  </channel>
</rss>