<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Connector for Expansion Header</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181235#M7715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please see MX5QSB HW use guide:&lt;/P&gt;&lt;P&gt;3.16. Expansion Header (J13)&lt;BR /&gt;A 120-pin Expansion Port Header is provided on the Quick Start board for use with many optionally&lt;BR /&gt;expansion boards available from Freescale, or for custom designed boards made be the developer. At&lt;BR /&gt;the time of initial production, the following expansion boards are available from Freescale:&lt;BR /&gt;• MCIMXHDMICARD HDMI signal output daughter card&lt;BR /&gt;• MCIMX28LCD 4.3” WVGA Touch Panel LCD Display&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The Expansion Port makes the following features of the i.MX53 Processor available to be used on a&lt;BR /&gt;custom built expansion card:&lt;BR /&gt;• Two Serial Peripheral Interfaces (SPI) CSPI, eCSDPI2&lt;BR /&gt;• Two I2S/SSI/AC97 Ports AUDMUX4, AUDMUX5&lt;BR /&gt;• Two Inter-Integrated Circuits (I2C) I2C1, I2C2&lt;BR /&gt;• 2 UARTs UART4, UART5&lt;BR /&gt;• SPDIF Audio&lt;BR /&gt;• USB ULPI Port USBH2&lt;BR /&gt;• 24-bit Data and display control signals&lt;BR /&gt;• Resistive Touch Screen Interface&lt;BR /&gt;• Various Voltage rails&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Oct 2011 16:19:22 GMT</pubDate>
    <dc:creator>LilyZhang</dc:creator>
    <dc:date>2011-10-31T16:19:22Z</dc:date>
    <item>
      <title>Connector for Expansion Header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181234#M7714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN id="result_box" lang="en" lang="en"&gt;&lt;SPAN class="hps"&gt;Hello,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;are&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;new to the forum&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and I apologize&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;for the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;bad English&lt;/SPAN&gt; &lt;SPAN class="atn hps"&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;for errors&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;is the fault of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;google translator&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;I would use&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the expansion port&lt;/SPAN&gt; (J13) &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;IMX53QSB&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;but&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;I do not know&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;where to find&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a suitable cable&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;for&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;that connector&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;Does anyone know&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;tell me&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;some website&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;where they sell&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;these cables&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;Thanks&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to all&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2011 13:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181234#M7714</guid>
      <dc:creator>FerdinandoCrisc</dc:creator>
      <dc:date>2011-10-31T13:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: Connector for Expansion Header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181235#M7715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please see MX5QSB HW use guide:&lt;/P&gt;&lt;P&gt;3.16. Expansion Header (J13)&lt;BR /&gt;A 120-pin Expansion Port Header is provided on the Quick Start board for use with many optionally&lt;BR /&gt;expansion boards available from Freescale, or for custom designed boards made be the developer. At&lt;BR /&gt;the time of initial production, the following expansion boards are available from Freescale:&lt;BR /&gt;• MCIMXHDMICARD HDMI signal output daughter card&lt;BR /&gt;• MCIMX28LCD 4.3” WVGA Touch Panel LCD Display&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The Expansion Port makes the following features of the i.MX53 Processor available to be used on a&lt;BR /&gt;custom built expansion card:&lt;BR /&gt;• Two Serial Peripheral Interfaces (SPI) CSPI, eCSDPI2&lt;BR /&gt;• Two I2S/SSI/AC97 Ports AUDMUX4, AUDMUX5&lt;BR /&gt;• Two Inter-Integrated Circuits (I2C) I2C1, I2C2&lt;BR /&gt;• 2 UARTs UART4, UART5&lt;BR /&gt;• SPDIF Audio&lt;BR /&gt;• USB ULPI Port USBH2&lt;BR /&gt;• 24-bit Data and display control signals&lt;BR /&gt;• Resistive Touch Screen Interface&lt;BR /&gt;• Various Voltage rails&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2011 16:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181235#M7715</guid>
      <dc:creator>LilyZhang</dc:creator>
      <dc:date>2011-10-31T16:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: Connector for Expansion Header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181236#M7716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN id="result_box" lang="en" lang="en"&gt;&lt;SPAN class="hps"&gt;Thanks&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;for your attention&lt;/SPAN&gt;&lt;SPAN&gt;, but&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;I have some doubts&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;MCIMXHDMICARD:&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;looking the&lt;/SPAN&gt; schematic &lt;SPAN class="hps"&gt;I can not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;tell&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN id="result_box" lang="en" lang="en"&gt;&lt;SPAN class="hps"&gt;if there are&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;any&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;pin&lt;/SPAN&gt; of the &lt;SPAN class="hps"&gt;expansion port&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;or only&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the pin of display&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;If&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;all pins&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;are present&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;what type&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of connector&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;you&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;want&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to use them&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;?&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;MCIMX28LCD&lt;/SPAN&gt;: &lt;/SPAN&gt;&lt;SPAN id="result_box" lang="en" lang="en"&gt;&lt;SPAN class="hps"&gt;would be ideal&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;because it&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;also includes the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;touch screen&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;but I can not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;find&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the schematic and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;can not figure out&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;if and how&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the pins&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;are brought to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the expansion port&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN id="result_box" lang="en" lang="en"&gt;&lt;BR /&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;thanks&lt;/SPAN&gt;&lt;/SPAN&gt; for help me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2011 16:48:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181236#M7716</guid>
      <dc:creator>FerdinandoCrisc</dc:creator>
      <dc:date>2011-10-31T16:48:47Z</dc:date>
    </item>
    <item>
      <title>Re: Connector for Expansion Header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181237#M7717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. &lt;SPAN class="hps"&gt;MCIMXHDMICARD: Please see the information under &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;tab=Buy_Parametric_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;tab=Buy_Parametric_Tab&lt;/A&gt;. I2C connection in Connector is for HDMI chip connection. DISP0_RESET is for HDMI reset signal etc.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;2. &lt;SPAN class="hps"&gt;MCIMX28LCD: Please get the information from &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;tab=Buy_Parametric_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;tab=Buy_Parametric_Tab&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2011 02:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connector-for-Expansion-Header/m-p/181237#M7717</guid>
      <dc:creator>LilyZhang</dc:creator>
      <dc:date>2011-11-01T02:15:00Z</dc:date>
    </item>
  </channel>
</rss>