<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is MFG Configuration required in Board configs to copy U-Boot alone? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483176#M77030</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You are right : it is not needed to change U-boot sources in order to&lt;/P&gt;&lt;P&gt;load U-boot binary image to memory. Looks like the i.MX6 in Your case &lt;/P&gt;&lt;P&gt;is not in serial (USB) boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Apr 2016 09:09:21 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-04-28T09:09:21Z</dc:date>
    <item>
      <title>Is MFG Configuration required in Board configs to copy U-Boot alone?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483175#M77029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've built U-boot.bin file for a customized board, taking sabreauto U-boot as reference.&lt;/P&gt;&lt;P&gt;Now i would like to copy U-boot binary to external RAM using MfG tool.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1). Is It required to configure MFG tool specific configuration in Board config files(.h &amp;amp; .c) to copy U-Boot binary alone?&lt;/P&gt;&lt;P&gt;(as far as i know, it is only required when we need to copy kernel along with u-boot).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm getting error when i try to load to eRAM, attached Mfg tool log. When i connect JTAG to see updated DCD values, &lt;/P&gt;&lt;P&gt;they are set to default values, not able to see updated values from imximage.cfg input file.&lt;/P&gt;&lt;P&gt;checked also in U-boot.bin file with editor tool, there is no mention about DCD registers, why so?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help, Thanks.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337032"&gt;MfgTool.log.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 13:40:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483175#M77029</guid>
      <dc:creator>maheshkumarkoda</dc:creator>
      <dc:date>2016-04-27T13:40:30Z</dc:date>
    </item>
    <item>
      <title>Re: Is MFG Configuration required in Board configs to copy U-Boot alone?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483176#M77030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You are right : it is not needed to change U-boot sources in order to&lt;/P&gt;&lt;P&gt;load U-boot binary image to memory. Looks like the i.MX6 in Your case &lt;/P&gt;&lt;P&gt;is not in serial (USB) boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 09:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483176#M77030</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-28T09:09:21Z</dc:date>
    </item>
    <item>
      <title>Re: Is MFG Configuration required in Board configs to copy U-Boot alone?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483177#M77031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have USB OTG(HID mode) to download U-boot.bin to eRAM and a serial port to see booting log in Console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect RAM is not initialized by DCD values(DCD is provided by hardware expert, so there may not be a problem with calibrated values).&lt;/P&gt;&lt;P&gt;However I would like to cross check DCD information in U-boot.bin once, Is there a way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 10:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483177#M77031</guid>
      <dc:creator>maheshkumarkoda</dc:creator>
      <dc:date>2016-04-28T10:06:53Z</dc:date>
    </item>
    <item>
      <title>Re: Is MFG Configuration required in Board configs to copy U-Boot alone?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483178#M77032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check if it is possible to load and run (NXP) U-boot on NXP board via&lt;/P&gt;&lt;P&gt;MFG.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; &lt;/P&gt;&lt;P&gt; RAM may be not initialized in secure boot, since IVT, DCD must be signed in such case.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2016 03:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-MFG-Configuration-required-in-Board-configs-to-copy-U-Boot/m-p/483178#M77032</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-05-04T03:28:05Z</dc:date>
    </item>
  </channel>
</rss>