<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 about i.mx6q boot question</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181150#M7700</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want boot i.mx6q_arm2 from sd,I use 4GB DDR3,8 chips,BSP is L3.0.15_12.05.01.&lt;BR /&gt;question:&lt;BR /&gt;1:system no boot when Temperature less than 43 C.(CPU is PCIMX6Q6AVT10AB)&lt;BR /&gt;boot logs:&lt;BR /&gt; U-Boot 2009.08 ( 8鏈?10 2012 - 18:44:25)&lt;BR /&gt; U-Boot code: 27800720 -&amp;gt; 27831000 BSS: -&amp;gt; 278664B4&lt;BR /&gt; CPU: Freescale i.MX6 family TO0.0 at 792 MHz&lt;BR /&gt; Temperature: 60 C, calibration data 0x5874de7d&lt;BR /&gt; .......&lt;BR /&gt;2:4GB DDR3 only find 2GB(BANK 1,DDR3 type is EDJ4216BASE )&lt;BR /&gt; I modify mx6q_arm.h &lt;BR /&gt; #define CONFIG_NR_DRAM_BANKS 2&lt;BR /&gt; #define PHYS_SDRAM_1 CSD0_DDR_BASE_ADDR&lt;BR /&gt; #define PHYS_SDRAM_1_SIZE (2u*1024*1024*1024)&lt;BR /&gt; #define PHYS_SDRAM_2 CSD1_DDR_BASE_ADDR&lt;BR /&gt; #define PHYS_SDRAM_2_SIZE (2u*1024*1024*1024)&lt;BR /&gt; #define iomem_valid_addr(addr,size) \&lt;BR /&gt; ((addr&amp;gt;=PHYS_SDRAM_1 &amp;amp;&amp;amp; addr&amp;lt;=(PHYS_SDRAM_1+PHYS_SDRAM_1_SIZE)) \&lt;BR /&gt; || (addr&amp;gt;=PHYS_SDRAM_2 &amp;amp;&amp;amp; addr&amp;lt;=(PHYS_SDRAM_2+PHYS_SDRAM_2_SIZE)))&lt;BR /&gt;boot logs: &lt;BR /&gt; Board: MX6Q/SDL-ARM2:[ POR ]&lt;BR /&gt; Boot Device: SD&lt;BR /&gt; I2C: ready&lt;BR /&gt; RAM Configuration:&lt;BR /&gt; Bank #0: 00000000 0 kB&lt;BR /&gt; Bank #1: 00000000 0 kB&lt;BR /&gt; RAM Configuration:&lt;BR /&gt; Bank #0: 10000000 2 GB&lt;BR /&gt; Bank #1: 00000000 0 kB&lt;BR /&gt;What is cause? please help me, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Aug 2012 11:37:03 GMT</pubDate>
    <dc:creator>tom_y</dc:creator>
    <dc:date>2012-08-10T11:37:03Z</dc:date>
    <item>
      <title>about i.mx6q boot question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181150#M7700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want boot i.mx6q_arm2 from sd,I use 4GB DDR3,8 chips,BSP is L3.0.15_12.05.01.&lt;BR /&gt;question:&lt;BR /&gt;1:system no boot when Temperature less than 43 C.(CPU is PCIMX6Q6AVT10AB)&lt;BR /&gt;boot logs:&lt;BR /&gt; U-Boot 2009.08 ( 8鏈?10 2012 - 18:44:25)&lt;BR /&gt; U-Boot code: 27800720 -&amp;gt; 27831000 BSS: -&amp;gt; 278664B4&lt;BR /&gt; CPU: Freescale i.MX6 family TO0.0 at 792 MHz&lt;BR /&gt; Temperature: 60 C, calibration data 0x5874de7d&lt;BR /&gt; .......&lt;BR /&gt;2:4GB DDR3 only find 2GB(BANK 1,DDR3 type is EDJ4216BASE )&lt;BR /&gt; I modify mx6q_arm.h &lt;BR /&gt; #define CONFIG_NR_DRAM_BANKS 2&lt;BR /&gt; #define PHYS_SDRAM_1 CSD0_DDR_BASE_ADDR&lt;BR /&gt; #define PHYS_SDRAM_1_SIZE (2u*1024*1024*1024)&lt;BR /&gt; #define PHYS_SDRAM_2 CSD1_DDR_BASE_ADDR&lt;BR /&gt; #define PHYS_SDRAM_2_SIZE (2u*1024*1024*1024)&lt;BR /&gt; #define iomem_valid_addr(addr,size) \&lt;BR /&gt; ((addr&amp;gt;=PHYS_SDRAM_1 &amp;amp;&amp;amp; addr&amp;lt;=(PHYS_SDRAM_1+PHYS_SDRAM_1_SIZE)) \&lt;BR /&gt; || (addr&amp;gt;=PHYS_SDRAM_2 &amp;amp;&amp;amp; addr&amp;lt;=(PHYS_SDRAM_2+PHYS_SDRAM_2_SIZE)))&lt;BR /&gt;boot logs: &lt;BR /&gt; Board: MX6Q/SDL-ARM2:[ POR ]&lt;BR /&gt; Boot Device: SD&lt;BR /&gt; I2C: ready&lt;BR /&gt; RAM Configuration:&lt;BR /&gt; Bank #0: 00000000 0 kB&lt;BR /&gt; Bank #1: 00000000 0 kB&lt;BR /&gt; RAM Configuration:&lt;BR /&gt; Bank #0: 10000000 2 GB&lt;BR /&gt; Bank #1: 00000000 0 kB&lt;BR /&gt;What is cause? please help me, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2012 11:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181150#M7700</guid>
      <dc:creator>tom_y</dc:creator>
      <dc:date>2012-08-10T11:37:03Z</dc:date>
    </item>
    <item>
      <title>Re: about i.mx6q boot question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181151#M7701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;second question is ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Aug 2012 06:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181151#M7701</guid>
      <dc:creator>tom_y</dc:creator>
      <dc:date>2012-08-11T06:23:29Z</dc:date>
    </item>
    <item>
      <title>Re: about i.mx6q boot question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181152#M7702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our internal LDO is&amp;nbsp;a bit&amp;nbsp;sensitive, output bulk capacitor must near the power pin very close, better within 100mil, refer oure SD Board design.&lt;/P&gt;&lt;P&gt;If you are debugging on our ARM2 CPU board, you may&amp;nbsp;remove the 22uF capacitor on ARM_CAP&amp;nbsp;to the back of CPU, weld it on the via.&lt;/P&gt;&lt;P&gt;Good Luck, waiting for your good news.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2012 10:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6q-boot-question/m-p/181152#M7702</guid>
      <dc:creator>fei_liu</dc:creator>
      <dc:date>2012-09-06T10:41:37Z</dc:date>
    </item>
  </channel>
</rss>