<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6Q :  How to work a Watchdog Timer in the on-chip boot ROM code ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482972#M76992</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;BR /&gt;I consider a Watchdog Timer (WDOG) behavior in the on-chip boot ROM code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In figure 8-2 Serial Download Boot Flow of IMX6DQRM Rev. 3,&lt;BR /&gt;it said ARM core will reset if no any activity within 90 seconds when WDOG_ENABLE=1. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Then, &lt;BR /&gt;do the WDOG External signals&amp;nbsp; ( WDOGx_B ,WDOGx_RESET_B_D ) connect to iMX6 I/O pad ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If Yes,&lt;BR /&gt;which pads are connected with WDOG External signals ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DISP0_DAT8 or GPIO_9 or SD1_DATA2 or DISP0_DAT9 or GPIO_1 or SD1_DATA3 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Mar 2016 04:09:51 GMT</pubDate>
    <dc:creator>koichisakagami</dc:creator>
    <dc:date>2016-03-17T04:09:51Z</dc:date>
    <item>
      <title>iMX6Q :  How to work a Watchdog Timer in the on-chip boot ROM code ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482972#M76992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;BR /&gt;I consider a Watchdog Timer (WDOG) behavior in the on-chip boot ROM code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In figure 8-2 Serial Download Boot Flow of IMX6DQRM Rev. 3,&lt;BR /&gt;it said ARM core will reset if no any activity within 90 seconds when WDOG_ENABLE=1. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Then, &lt;BR /&gt;do the WDOG External signals&amp;nbsp; ( WDOGx_B ,WDOGx_RESET_B_D ) connect to iMX6 I/O pad ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If Yes,&lt;BR /&gt;which pads are connected with WDOG External signals ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DISP0_DAT8 or GPIO_9 or SD1_DATA2 or DISP0_DAT9 or GPIO_1 or SD1_DATA3 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 04:09:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482972#M76992</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2016-03-17T04:09:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q :  How to work a Watchdog Timer in the on-chip boot ROM code ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482973#M76993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Koichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;out of reset state of these pads are described in&lt;/P&gt;&lt;P&gt;Table 100. 21 x 21 mm Functional Contact Assignments i.MX6DQ Datasheet &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6DQCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;ROM does not configure wdog external signals Upon timeout, the wdog just &lt;/P&gt;&lt;P&gt;asserts the internal system reset signal, WDOG_RESET_B_DEB &lt;/P&gt;&lt;P&gt;to the System Reset Controller (SRC).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 07:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482973#M76993</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-17T07:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q :  How to work a Watchdog Timer in the on-chip boot ROM code ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482974#M76994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor san,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 00:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-How-to-work-a-Watchdog-Timer-in-the-on-chip-boot-ROM-code/m-p/482974#M76994</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2016-03-18T00:19:24Z</dc:date>
    </item>
  </channel>
</rss>