<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DDR reserved bits cleared during boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-reserved-bits-cleared-during-boot/m-p/482954#M76983</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have small question about reserved bits in DDR subsystem.&lt;/P&gt;&lt;P&gt;Let's use i.MX6Q sabre board (mx6qsabresd) , and nearly any Linux SDK.&lt;/P&gt;&lt;P&gt;Let's picup some register, for example IOMUXC_SW_PAD_CTL_PAD_DRAM_ODT0 (0x020e059c), but there are others with same problem.&lt;/P&gt;&lt;P&gt;In documentation there is that reset value is &lt;STRONG&gt;0x0000&lt;SPAN style="text-decoration: underline;"&gt;3&lt;/SPAN&gt;030&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In U-boot there are records in *.cfg files (for device configuration block - ROM init) like&lt;/P&gt;&lt;P&gt;DATA 4, 0x020e059c, &lt;STRONG&gt;0x0000&lt;SPAN style="text-decoration: underline;"&gt;0&lt;/SPAN&gt;030&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;So this will set DSE value of pin, but also clears reserved bits (&lt;STRONG&gt;bits 15-12&lt;/STRONG&gt;) during ddr init by rom code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it correct to clear these reserved bits? Are they useful for anything?&lt;/P&gt;&lt;P&gt;And is it safe to clear them?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 14:04:36 GMT</pubDate>
    <dc:creator>pavelstanek</dc:creator>
    <dc:date>2016-04-05T14:04:36Z</dc:date>
    <item>
      <title>DDR reserved bits cleared during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-reserved-bits-cleared-during-boot/m-p/482954#M76983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have small question about reserved bits in DDR subsystem.&lt;/P&gt;&lt;P&gt;Let's use i.MX6Q sabre board (mx6qsabresd) , and nearly any Linux SDK.&lt;/P&gt;&lt;P&gt;Let's picup some register, for example IOMUXC_SW_PAD_CTL_PAD_DRAM_ODT0 (0x020e059c), but there are others with same problem.&lt;/P&gt;&lt;P&gt;In documentation there is that reset value is &lt;STRONG&gt;0x0000&lt;SPAN style="text-decoration: underline;"&gt;3&lt;/SPAN&gt;030&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In U-boot there are records in *.cfg files (for device configuration block - ROM init) like&lt;/P&gt;&lt;P&gt;DATA 4, 0x020e059c, &lt;STRONG&gt;0x0000&lt;SPAN style="text-decoration: underline;"&gt;0&lt;/SPAN&gt;030&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;So this will set DSE value of pin, but also clears reserved bits (&lt;STRONG&gt;bits 15-12&lt;/STRONG&gt;) during ddr init by rom code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it correct to clear these reserved bits? Are they useful for anything?&lt;/P&gt;&lt;P&gt;And is it safe to clear them?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 14:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-reserved-bits-cleared-during-boot/m-p/482954#M76983</guid>
      <dc:creator>pavelstanek</dc:creator>
      <dc:date>2016-04-05T14:04:36Z</dc:date>
    </item>
    <item>
      <title>Re: DDR reserved bits cleared during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-reserved-bits-cleared-during-boot/m-p/482955#M76984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; The reserved bits concern with preliminary i.MX6 specs, where PUE and PKE &lt;BR /&gt;bits were used (to define pull up options). Strictly speaking, initialization code should&lt;/P&gt;&lt;P&gt;follow recent RM recommendations. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 09:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-reserved-bits-cleared-during-boot/m-p/482955#M76984</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-06T09:07:02Z</dc:date>
    </item>
  </channel>
</rss>