<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBSP 3.14.28: building galcore kernel module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BSP-3-14-28-building-galcore-kernel-module/m-p/481962#M76819</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build a "galcore.ko" module in 3.14.28 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set "CONFIG_MXC_GPU_VIV=m".&lt;/P&gt;&lt;P&gt;I could do "bitbake linux-imx -c compile -f"&lt;/P&gt;&lt;P&gt;Then I did "bitbake linux-imx -c compile_kernelmodules"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: "v7_dma_flush_range" [drivers/mxc/gpu-viv/galcore.ko] undefined!&lt;/P&gt;&lt;P&gt;ERROR: "v7_dma_map_area" [drivers/mxc/gpu-viv/galcore.ko] undefined!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need separate galcore module in order to pass parameters such as contiguousBase and contiguousSize to galcore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to set these parameters in built-in galcore?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;N.S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Apr 2016 04:41:43 GMT</pubDate>
    <dc:creator>norishinozaki</dc:creator>
    <dc:date>2016-04-27T04:41:43Z</dc:date>
    <item>
      <title>BSP 3.14.28: building galcore kernel module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BSP-3-14-28-building-galcore-kernel-module/m-p/481962#M76819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build a "galcore.ko" module in 3.14.28 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set "CONFIG_MXC_GPU_VIV=m".&lt;/P&gt;&lt;P&gt;I could do "bitbake linux-imx -c compile -f"&lt;/P&gt;&lt;P&gt;Then I did "bitbake linux-imx -c compile_kernelmodules"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: "v7_dma_flush_range" [drivers/mxc/gpu-viv/galcore.ko] undefined!&lt;/P&gt;&lt;P&gt;ERROR: "v7_dma_map_area" [drivers/mxc/gpu-viv/galcore.ko] undefined!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need separate galcore module in order to pass parameters such as contiguousBase and contiguousSize to galcore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to set these parameters in built-in galcore?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;N.S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 04:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BSP-3-14-28-building-galcore-kernel-module/m-p/481962#M76819</guid>
      <dc:creator>norishinozaki</dc:creator>
      <dc:date>2016-04-27T04:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: BSP 3.14.28: building galcore kernel module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BSP-3-14-28-building-galcore-kernel-module/m-p/481963#M76820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;according to the Linux reference manual,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;13.1.1.6 Menu Configuration Options&lt;/P&gt;&lt;P&gt;The following Linux kernel configurations are provided for GPU driver:&lt;/P&gt;&lt;P&gt;• CONFIG_MXC_GPU_VIV is a configuration option for GPU driver. In the&lt;/P&gt;&lt;P&gt;menuconfig this option is available under Device Drivers &amp;gt; MXC support drivers &amp;gt;&lt;/P&gt;&lt;P&gt;MXC Vivante GPU support &amp;gt; MXC Vivante GPU support.&lt;/P&gt;&lt;P&gt;To get to the GPU library package in Yocto, use the command bitbake linux-imx -c&lt;/P&gt;&lt;P&gt;menuconfig. On the screen displayed, select Configure the kernel and select "Device&lt;/P&gt;&lt;P&gt;Drivers" &amp;gt; "MXC support drivers" &amp;gt; "MXC Vivante GPU support" &amp;gt; "MXC Vivante&lt;/P&gt;&lt;P&gt;GPU support"and exit. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 03:51:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BSP-3-14-28-building-galcore-kernel-module/m-p/481963#M76820</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2016-05-03T03:51:05Z</dc:date>
    </item>
  </channel>
</rss>