<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Recommended Yocto project image for UART console? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Recommended-Yocto-project-image-for-UART-console/m-p/481200#M76726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am building U-boot using Yocto project to boot up my Custom board, With U-boot basic initialization I like to download customized Bootloader in next level, I want to know recommended image name for enabling UART console to see feedback from the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I came across two Image names:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1). core-image-minimal : A small image that only allows a device to boot.&lt;/P&gt;&lt;P&gt;2). core-image-base : A console only image that fully supports the target device hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess i can use core-image-base? If yes, does it take longer booting time than core-image-minimal?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Mar 2016 11:19:38 GMT</pubDate>
    <dc:creator>maheshkumarkoda</dc:creator>
    <dc:date>2016-03-16T11:19:38Z</dc:date>
    <item>
      <title>Recommended Yocto project image for UART console?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recommended-Yocto-project-image-for-UART-console/m-p/481200#M76726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am building U-boot using Yocto project to boot up my Custom board, With U-boot basic initialization I like to download customized Bootloader in next level, I want to know recommended image name for enabling UART console to see feedback from the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I came across two Image names:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1). core-image-minimal : A small image that only allows a device to boot.&lt;/P&gt;&lt;P&gt;2). core-image-base : A console only image that fully supports the target device hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess i can use core-image-base? If yes, does it take longer booting time than core-image-minimal?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 11:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recommended-Yocto-project-image-for-UART-console/m-p/481200#M76726</guid>
      <dc:creator>maheshkumarkoda</dc:creator>
      <dc:date>2016-03-16T11:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: Recommended Yocto project image for UART console?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recommended-Yocto-project-image-for-UART-console/m-p/481201#M76727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mahesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;both have uart console but since core-image-minimal is smaller&lt;/P&gt;&lt;P&gt;less boot time can be expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 11:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recommended-Yocto-project-image-for-UART-console/m-p/481201#M76727</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-16T11:33:36Z</dc:date>
    </item>
  </channel>
</rss>