<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6 vpu firmware source code</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480887#M76630</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I are developing an encoding application on i.MX6Q Sabre board using Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga). &lt;/P&gt;&lt;P&gt;I would like to change rate control (quant param control) of macro-block level.&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I think that it is necessary to change the firmware of the &lt;SPAN&gt;VPU. But, there are only a binary file (vpu_fw_imx6q.bin) of the firmware in yocto project.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Can I get the source code of VPU firmware or sample code from somewhere?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kenji&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 09:46:53 GMT</pubDate>
    <dc:creator>teranishi_kenji</dc:creator>
    <dc:date>2016-04-05T09:46:53Z</dc:date>
    <item>
      <title>i.MX6 vpu firmware source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480887#M76630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I are developing an encoding application on i.MX6Q Sabre board using Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga). &lt;/P&gt;&lt;P&gt;I would like to change rate control (quant param control) of macro-block level.&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I think that it is necessary to change the firmware of the &lt;SPAN&gt;VPU. But, there are only a binary file (vpu_fw_imx6q.bin) of the firmware in yocto project.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Can I get the source code of VPU firmware or sample code from somewhere?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kenji&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 09:46:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480887#M76630</guid>
      <dc:creator>teranishi_kenji</dc:creator>
      <dc:date>2016-04-05T09:46:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 vpu firmware source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480888#M76631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kenji Teranishi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately only the binaries are provided but an API is provided in order to work with the VPU firmware. You may find the following thread useful:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/397728#comment-397728" title="https://community.freescale.com/message/397728#comment-397728"&gt;https://community.freescale.com/message/397728&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 21:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480888#M76631</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-04-05T21:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 vpu firmware source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480889#M76632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gusarambula,&lt;/P&gt;&lt;P&gt;Thank you for your comment.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;I saw the API. However, there are no macro-block level API.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;In other words, are there no m&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;ethod for setting macro-block's quant param?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 05:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-vpu-firmware-source-code/m-p/480889#M76632</guid>
      <dc:creator>teranishi_kenji</dc:creator>
      <dc:date>2016-04-06T05:08:53Z</dc:date>
    </item>
  </channel>
</rss>