<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RNDIS Support in imx6_kernel for Android 4.4.3 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RNDIS-Support-in-imx6-kernel-for-Android-4-4-3/m-p/480417#M76514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when i connect usb to ethernet converter with otg USB of sabresd platform, it does not create any interface like usb0.&lt;/P&gt;&lt;P&gt;Where as when i check same converter with some other android board it shown interface usb0.&lt;/P&gt;&lt;P&gt;I am checking interface name using netcfg command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also i have checked in kernel configuration to enable RNDIS mode but that option is not present in make menuconfig interface in imx6 kernel.&lt;/P&gt;&lt;P&gt;where as using beagle board kernel is supporting RNDIS mode and that option is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do i add its driver in kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 May 2016 10:21:28 GMT</pubDate>
    <dc:creator>bqam</dc:creator>
    <dc:date>2016-05-18T10:21:28Z</dc:date>
    <item>
      <title>RNDIS Support in imx6_kernel for Android 4.4.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RNDIS-Support-in-imx6-kernel-for-Android-4-4-3/m-p/480417#M76514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when i connect usb to ethernet converter with otg USB of sabresd platform, it does not create any interface like usb0.&lt;/P&gt;&lt;P&gt;Where as when i check same converter with some other android board it shown interface usb0.&lt;/P&gt;&lt;P&gt;I am checking interface name using netcfg command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also i have checked in kernel configuration to enable RNDIS mode but that option is not present in make menuconfig interface in imx6 kernel.&lt;/P&gt;&lt;P&gt;where as using beagle board kernel is supporting RNDIS mode and that option is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do i add its driver in kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 May 2016 10:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RNDIS-Support-in-imx6-kernel-for-Android-4-4-3/m-p/480417#M76514</guid>
      <dc:creator>bqam</dc:creator>
      <dc:date>2016-05-18T10:21:28Z</dc:date>
    </item>
  </channel>
</rss>