<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Frame buffer resolution in i.Mx6 Yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Frame-buffer-resolution-in-i-Mx6-Yocto/m-p/480367#M76498</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can change virtual resolution with the command like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# fbset -vxres 800 -vyres 480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jan 2016 05:49:03 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-01-12T05:49:03Z</dc:date>
    <item>
      <title>Frame buffer resolution in i.Mx6 Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-buffer-resolution-in-i-Mx6-Yocto/m-p/480366#M76497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using i.Mx6Q processor with the Yocto BSP release of &lt;SPAN style="color: #3334ca;"&gt;fsl-yocto-L3.14.38_6qp-ga&lt;/SPAN&gt; (&lt;SPAN style="color: #3334ca;"&gt;imx-3.14.38-6QP_ga&lt;/SPAN&gt;). I have tried to Launch the Yocto filesystem in my customized platform with GUI in my LCD-display (800x480). While dumping any image into it, the image is not properly visible.&lt;/P&gt;&lt;P&gt;I have found that there is a change in the virtual X/Y resolution of display. Below is the command executed to check the same:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;root@board:~# &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;root@board:~# fbset&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;mode "800x480-60"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; # D: 33.260 MHz, H: 31.496 kHz, V: 59.993 Hz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; geometry 800 480 &lt;SPAN style="color: #e23d39;"&gt;832 512&lt;/SPAN&gt; 16&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; timings 30066 88 40 33 10 128 2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; rgba 5/11,6/5,5/0,0/0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;endmode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3334ca;"&gt;root@board:~#&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here the virtual X/Y resolution is increased by 32 (&lt;SPAN style="color: #e23d39;"&gt;832 512&lt;/SPAN&gt;) instead of (&lt;SPAN style="color: #3334ca;"&gt;800 480&lt;/SPAN&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it even number aligned resolution?. Please suggest me to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Salih&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Dec 2015 09:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-buffer-resolution-in-i-Mx6-Yocto/m-p/480366#M76497</guid>
      <dc:creator>MuhammadhSalih</dc:creator>
      <dc:date>2015-12-12T09:46:28Z</dc:date>
    </item>
    <item>
      <title>Re: Frame buffer resolution in i.Mx6 Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-buffer-resolution-in-i-Mx6-Yocto/m-p/480367#M76498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can change virtual resolution with the command like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# fbset -vxres 800 -vyres 480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 05:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-buffer-resolution-in-i-Mx6-Yocto/m-p/480367#M76498</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-01-12T05:49:03Z</dc:date>
    </item>
  </channel>
</rss>