<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 Open-Drain maximum rating in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480282#M76462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; maximum allowed voltage on the pad is defined by&lt;/P&gt;&lt;P&gt;Datasheet Table 4. Absolute Maximum Ratings &lt;/P&gt;&lt;P&gt;Input/output voltage range :&amp;nbsp; OVDD+0.3V&amp;nbsp;&amp;nbsp; (OVDD is the I/O supply voltage.)&lt;/P&gt;&lt;P&gt;2. maximum allowed current through the output transistor is not defined by&lt;/P&gt;&lt;P&gt;datasheet. Limitation would be max. Junction temperature defined in&lt;/P&gt;&lt;P&gt;Table 6. Operating Ranges&lt;/P&gt;&lt;P&gt;Note output transistor impedance may be affected by DSE, defined in&lt;/P&gt;&lt;P&gt;Table 33,34 GPIO Output Buffer Average Impedance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Apr 2016 00:36:32 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-04-06T00:36:32Z</dc:date>
    <item>
      <title>iMX6 Open-Drain maximum rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480281#M76461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to connect a PWM output using open-drain pad configuration.&amp;nbsp; The PWM bank voltage is 1.8V.&lt;/P&gt;&lt;P&gt;I couldn't find the information I need in the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone answer :&lt;/P&gt;&lt;P&gt;1. In open-drain configuration, what is the maximum allowed external voltage on the pad?&lt;/P&gt;&lt;P&gt;2. What is the maximum allowed current through the internal transistor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 13:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480281#M76461</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2016-04-05T13:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Open-Drain maximum rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480282#M76462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; maximum allowed voltage on the pad is defined by&lt;/P&gt;&lt;P&gt;Datasheet Table 4. Absolute Maximum Ratings &lt;/P&gt;&lt;P&gt;Input/output voltage range :&amp;nbsp; OVDD+0.3V&amp;nbsp;&amp;nbsp; (OVDD is the I/O supply voltage.)&lt;/P&gt;&lt;P&gt;2. maximum allowed current through the output transistor is not defined by&lt;/P&gt;&lt;P&gt;datasheet. Limitation would be max. Junction temperature defined in&lt;/P&gt;&lt;P&gt;Table 6. Operating Ranges&lt;/P&gt;&lt;P&gt;Note output transistor impedance may be affected by DSE, defined in&lt;/P&gt;&lt;P&gt;Table 33,34 GPIO Output Buffer Average Impedance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 00:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480282#M76462</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-06T00:36:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Open-Drain maximum rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480283#M76463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the prompt reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw the OVDD+0.3 spec in the Absolute Maximum Ratings table. However, I have doubt that it is correct for Open-Drain configuration.&amp;nbsp; I think OVDD+0.3 is the limit for Totem-Pole configuration.&lt;/P&gt;&lt;P&gt;Open-Drain is used very frequently for simple level-shifting is slow signals. I need to upshift from 1.8V to 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any way to verify this with the h/w team?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 05:48:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480283#M76463</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2016-04-06T05:48:30Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Open-Drain maximum rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480284#M76464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this is correct. Note also there is esd protection&lt;/P&gt;&lt;P&gt;diode on pad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 06:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Open-Drain-maximum-rating/m-p/480284#M76464</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-06T06:37:21Z</dc:date>
    </item>
  </channel>
</rss>