<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to setup boot_data2 of plugin mode in u-boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-boot-data2-of-plugin-mode-in-u-boot/m-p/479571#M76323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on an imx.6 DL board bring-up using BSP l5.0.0_1.0.0-ga.&lt;/P&gt;&lt;P&gt;We need initialize the MMDC in plugin mode, but the parameters such as ivt_header, boot_data in mx6_plugin.S are all set to 0x0 by default.&lt;/P&gt;&lt;P&gt;I have tried to compile and run u-boot with CONFIG_USE_PLUGIN enabled on SabreSD demo board but no success to boot up.&lt;/P&gt;&lt;P&gt;Compared with old flash_header.s of u-boot v-2009, I think the ivt_header, boot_data, app_code_jump_v etc. are missing in l5.0.0_1.0.0-ga and later BSP.&lt;/P&gt;&lt;P&gt;Dose anyone can help to provide these parameters in plugin mode?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Mar 2016 03:19:55 GMT</pubDate>
    <dc:creator>mmj</dc:creator>
    <dc:date>2016-03-16T03:19:55Z</dc:date>
    <item>
      <title>How to setup boot_data2 of plugin mode in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-boot-data2-of-plugin-mode-in-u-boot/m-p/479571#M76323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on an imx.6 DL board bring-up using BSP l5.0.0_1.0.0-ga.&lt;/P&gt;&lt;P&gt;We need initialize the MMDC in plugin mode, but the parameters such as ivt_header, boot_data in mx6_plugin.S are all set to 0x0 by default.&lt;/P&gt;&lt;P&gt;I have tried to compile and run u-boot with CONFIG_USE_PLUGIN enabled on SabreSD demo board but no success to boot up.&lt;/P&gt;&lt;P&gt;Compared with old flash_header.s of u-boot v-2009, I think the ivt_header, boot_data, app_code_jump_v etc. are missing in l5.0.0_1.0.0-ga and later BSP.&lt;/P&gt;&lt;P&gt;Dose anyone can help to provide these parameters in plugin mode?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 03:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-boot-data2-of-plugin-mode-in-u-boot/m-p/479571#M76323</guid>
      <dc:creator>mmj</dc:creator>
      <dc:date>2016-03-16T03:19:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup boot_data2 of plugin mode in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-boot-data2-of-plugin-mode-in-u-boot/m-p/479572#M76324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;You can refer to &lt;A href="https://community.nxp.com/thread/337413"&gt;iMX6 - MFG-Tool firmware u-boot compiled in plugin mode&lt;/A&gt; . Hope this can do some help to you.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Apr 2016 11:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-boot-data2-of-plugin-mode-in-u-boot/m-p/479572#M76324</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2016-04-08T11:02:14Z</dc:date>
    </item>
  </channel>
</rss>