<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGPU hang</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPU-hang/m-p/479401#M76274</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running Kernel 3.14.28 on a custom imx6q-based board and I'm having the following problem with the GPU:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[galcore]: GPU[0] hang, automatic recovery.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once recovery is complete things work. Anyway, recovery causes HMI unavailability...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;1. What is going on with the GPU to have a GPU hang?&lt;/P&gt;&lt;P&gt;2. Is there some recent change/patch which addresses this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Feb 2016 14:12:32 GMT</pubDate>
    <dc:creator>Salvatore1z</dc:creator>
    <dc:date>2016-02-01T14:12:32Z</dc:date>
    <item>
      <title>GPU hang</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-hang/m-p/479401#M76274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running Kernel 3.14.28 on a custom imx6q-based board and I'm having the following problem with the GPU:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[galcore]: GPU[0] hang, automatic recovery.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once recovery is complete things work. Anyway, recovery causes HMI unavailability...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;1. What is going on with the GPU to have a GPU hang?&lt;/P&gt;&lt;P&gt;2. Is there some recent change/patch which addresses this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 14:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-hang/m-p/479401#M76274</guid>
      <dc:creator>Salvatore1z</dc:creator>
      <dc:date>2016-02-01T14:12:32Z</dc:date>
    </item>
    <item>
      <title>Re: GPU hang</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-hang/m-p/479402#M76275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; You may try the recent BSP L3.14.52, where GPU driver is&amp;nbsp; upgraded to Vivante v5.0.11p7.4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS" rel="nofollow"&gt;http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary Page :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW" rel="nofollow"&gt;i.MX 6 Series Software and Development Tool|NXP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Feb 2016 01:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-hang/m-p/479402#M76275</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-02T01:58:32Z</dc:date>
    </item>
  </channel>
</rss>