<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックno pull down on LCD_RS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479221#M76222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question about the LCD_RS pin on the i.MX28.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the ENABLE_PIN_BOOT_CHECK is blown and LCD_RS is NOT pulled down, and is connected to an LCD(LCD_DOTCLK),&amp;nbsp; is the boot mode guaranteed to be determined by the OTP eFuse bits in ROM0 (HW_OCOTP_ROM0:0x8002C1A0:31:24)?&amp;nbsp; There is not a pull-up on LCD_RS either. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a module with a i.MX28 chip that is used in two different base-boards.&amp;nbsp; One base-board pulls down LCD_RS and the other does not.&amp;nbsp; Both base-boards use this pin for LCD_DOTCLK for it's display.&amp;nbsp; Both of these configurations are reading the OTP eFuse bits, which is the way we expect them both to operate.&amp;nbsp; I need to know if the base-board that doesn't pull down LCD_RS is guaranteed?&amp;nbsp; The reason we need this to operate without a pull down is for cross-base-board compatibility.&amp;nbsp; We have thousands of boards without a pull down on LCD_RS that originally did not need the ENABLE_PIN_BOOT_CHECK to be blown, but now require it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JJ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Mar 2016 13:57:32 GMT</pubDate>
    <dc:creator>jjkropp-Triton</dc:creator>
    <dc:date>2016-03-15T13:57:32Z</dc:date>
    <item>
      <title>no pull down on LCD_RS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479221#M76222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question about the LCD_RS pin on the i.MX28.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the ENABLE_PIN_BOOT_CHECK is blown and LCD_RS is NOT pulled down, and is connected to an LCD(LCD_DOTCLK),&amp;nbsp; is the boot mode guaranteed to be determined by the OTP eFuse bits in ROM0 (HW_OCOTP_ROM0:0x8002C1A0:31:24)?&amp;nbsp; There is not a pull-up on LCD_RS either. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a module with a i.MX28 chip that is used in two different base-boards.&amp;nbsp; One base-board pulls down LCD_RS and the other does not.&amp;nbsp; Both base-boards use this pin for LCD_DOTCLK for it's display.&amp;nbsp; Both of these configurations are reading the OTP eFuse bits, which is the way we expect them both to operate.&amp;nbsp; I need to know if the base-board that doesn't pull down LCD_RS is guaranteed?&amp;nbsp; The reason we need this to operate without a pull down is for cross-base-board compatibility.&amp;nbsp; We have thousands of boards without a pull down on LCD_RS that originally did not need the ENABLE_PIN_BOOT_CHECK to be blown, but now require it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JJ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 13:57:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479221#M76222</guid>
      <dc:creator>jjkropp-Triton</dc:creator>
      <dc:date>2016-03-15T13:57:32Z</dc:date>
    </item>
    <item>
      <title>Re: no pull down on LCD_RS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479222#M76223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it has not pull resistor, only keeper, pads with pull resistors are described in&lt;/P&gt;&lt;P&gt;Table 9-3. i.MX28 Functions with Pullup Resistors i.MX28 Reference Manual (rev.1, 9/2010)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fdsp%2Fdoc%2Fref_manual%2FMCIMX28RM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 00:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479222#M76223</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-16T00:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: no pull down on LCD_RS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479223#M76224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response.&lt;/P&gt;&lt;P&gt;My question in about an external pull-down resistor on LCD_RS.&lt;/P&gt;&lt;P&gt;In reference to section 12.2.1. and Table 12.9.  ENABLE_PIN_BOOT_CHECK is blown.&lt;/P&gt;&lt;P&gt;We don’t have an external pull-down resistor (nor a pull-up) on LCD_RS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it ok to NOT have a pull-down resistor on LCD_RS?&lt;/P&gt;&lt;P&gt;Is the boot mode determined(guaranteed) by the OTP eFUSE bits without it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m asking this question because one of our designs has no pull down on LCD_RS and we need to read the boot mode from the eFUSE bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JJ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section 12.2.1 reads as follows:&lt;/P&gt;&lt;P&gt;If LCD_RS is pulled down, then the boot mode is determined by the OTP eFuse bits, as&lt;/P&gt;&lt;P&gt;defined in Table 12-4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 13:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479223#M76224</guid>
      <dc:creator>jjkropp-Triton</dc:creator>
      <dc:date>2016-03-16T13:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: no pull down on LCD_RS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479224#M76225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to i.MX28 design checklist&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-98792"&gt;Hardware Design Checklist for i.MX28&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the ENABLE_PIN_BOOT_CHECK OTP bit is blown, &lt;/P&gt;&lt;P&gt;LCD_RS is high -&amp;gt; check boot mode on LCD_D[5:0]&lt;/P&gt;&lt;P&gt;LCD_RS is low -&amp;gt; check boot mode on OTP bits&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 14:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479224#M76225</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-16T14:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: no pull down on LCD_RS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479225#M76226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the Gate keeper sufficient for LCD_RS low without adding an external pull-down resistor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JJ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 14:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479225#M76226</guid>
      <dc:creator>jjkropp-Triton</dc:creator>
      <dc:date>2016-03-16T14:22:49Z</dc:date>
    </item>
    <item>
      <title>Re: no pull down on LCD_RS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479226#M76227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;keeper just prevents pad from floating, I believe&lt;/P&gt;&lt;P&gt;it is not reliable solution for such purpose.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 01:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-pull-down-on-LCD-RS/m-p/479226#M76227</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-17T01:42:55Z</dc:date>
    </item>
  </channel>
</rss>