<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Audio issue in imx6q (linux-imx) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479177#M76201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt; I have added ssi block in DTS tree. I have also verified from dmesg logs that ssi block is getting initialized correctly. From the above logs shared, last line suggests error in DMA or IRQ. How can I check this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 14:48:44 GMT</pubDate>
    <dc:creator>sharvari</dc:creator>
    <dc:date>2016-04-26T14:48:44Z</dc:date>
    <item>
      <title>Audio issue in imx6q (linux-imx)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479175#M76199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am working on a custom board based on imx6q-arm2 board. I have linux-imx 3.14.28 running on it. I am facing an issue in AUDIO. My board has TLV codec interfaced via audmux to ssi. When i use aplay command , it shows the error as&lt;/P&gt;&lt;P&gt;aplay: pcm_write:1947: write error: Input/output error&lt;/P&gt;&lt;P&gt;and dmesg shows&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 6834.037168] imx-sdma 20ec000.sdma: wml = 0x0000001a&lt;/P&gt;&lt;P&gt;[ 6834.037181] imx-sdma 20ec000.sdma: shp_addr = 0x02028000&lt;/P&gt;&lt;P&gt;[ 6834.037193] imx-sdma 20ec000.sdma: per_addr = 0x00000000&lt;/P&gt;&lt;P&gt;[ 6834.037205] imx-sdma 20ec000.sdma: event_mask0 = 0x00000000&lt;/P&gt;&lt;P&gt;[ 6834.037217] imx-sdma 20ec000.sdma: event_mask1 = 0x00000040&lt;/P&gt;&lt;P&gt;[ 6834.037244] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 0: count: 16384 dma: 0x4c7c0000&amp;nbsp; intr&lt;/P&gt;&lt;P&gt;[ 6834.037261] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 1: count: 16384 dma: 0x4c7c4000&amp;nbsp; intr&lt;/P&gt;&lt;P&gt;[ 6834.037277] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 2: count: 16384 dma: 0x4c7c8000&amp;nbsp; intr&lt;/P&gt;&lt;P&gt;[ 6834.037293] imx-sdma 20ec000.sdma: sdma_prep_dma_cyclic :entry 3: count: 16384 dma: 0x4c7cc000 wrap intr&lt;/P&gt;&lt;P&gt;[ 6844.037593] ALSA sound/core/pcm_lib.c:1947 playback write error (DMA or IRQ trouble?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So what exactly can be the cause of this error.&lt;/P&gt;&lt;P&gt;If i use aplay -M test.wav , this playback error does not show up. but still sound can not be heard. Also with -M option, aplay never exists.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari Harisangam.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 12:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479175#M76199</guid>
      <dc:creator>sharvari</dc:creator>
      <dc:date>2016-04-26T12:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: Audio issue in imx6q (linux-imx)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479176#M76200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sharvari&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems dts files for arm2 board, like imx6q-arm2.dts, do not have&lt;/P&gt;&lt;P&gt;ssi entries. Suggest to add them using SabreSD dts examples&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_3.14.28_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_3.14.28_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 13:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479176#M76200</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-26T13:14:17Z</dc:date>
    </item>
    <item>
      <title>Re: Audio issue in imx6q (linux-imx)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479177#M76201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt; I have added ssi block in DTS tree. I have also verified from dmesg logs that ssi block is getting initialized correctly. From the above logs shared, last line suggests error in DMA or IRQ. How can I check this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 14:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479177#M76201</guid>
      <dc:creator>sharvari</dc:creator>
      <dc:date>2016-04-26T14:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: Audio issue in imx6q (linux-imx)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479178#M76202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sharvari&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check the LRCLK, MCLK and Bitclock using scope.&lt;/P&gt;&lt;P&gt;i.MX6 is configured in master or slave mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 03:44:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-issue-in-imx6q-linux-imx/m-p/479178#M76202</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2016-04-27T03:44:27Z</dc:date>
    </item>
  </channel>
</rss>