<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IPU alpha blending in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478923#M76154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Usually alpha blending is made on display processor (DP). As the only output of DP is the display, this will not be an option for you.&lt;/P&gt;&lt;P&gt;You could combine the images using VDIC (Video de-interlace) and send the result to display and other memory location. You will need to implement it on kernel, IPU driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 13:32:51 GMT</pubDate>
    <dc:creator>rogerio_silva</dc:creator>
    <dc:date>2016-04-05T13:32:51Z</dc:date>
    <item>
      <title>IPU alpha blending</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478922#M76153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using i.Mx6 based processor and my doubt is that.&lt;/P&gt;&lt;P&gt;Is it possible to both display in fb0 and save the output buffer to a file at the same time .&lt;/P&gt;&lt;P&gt;When i tried to do so i get segmentation fault.Is there something that am missing. Can Any one help me as am new to IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 11:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478922#M76153</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2016-04-04T11:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: IPU alpha blending</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478923#M76154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Usually alpha blending is made on display processor (DP). As the only output of DP is the display, this will not be an option for you.&lt;/P&gt;&lt;P&gt;You could combine the images using VDIC (Video de-interlace) and send the result to display and other memory location. You will need to implement it on kernel, IPU driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 13:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478923#M76154</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2016-04-05T13:32:51Z</dc:date>
    </item>
    <item>
      <title>Re: IPU alpha blending</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478924#M76155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seems that you can use Gstreamer for that. For more information, please refer to the Chapter 7 "Multimedia" of the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 08:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-alpha-blending/m-p/478924#M76155</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-04-11T08:03:08Z</dc:date>
    </item>
  </channel>
</rss>