<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX6UL HAB Questions</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-HAB-Questions/m-p/478545#M76060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the signed u-boot image be verified on the EVK without CLOSING the SoC&lt;/P&gt;&lt;P&gt;when loading via USB (mfgtools technique)? When attempting this I&lt;/P&gt;&lt;P&gt;consistently see HAB events with INV_ADDRESS CTX_AUTHENTICATION. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the binary CSF file created using the cst tool have to be padded to the&lt;/P&gt;&lt;P&gt;size specified with CONFIG_CSF_SIZE in the u-boot imximage.cfg file before&lt;/P&gt;&lt;P&gt;being appended to the u-boot image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the signed u-boot image need to be padded for 0x1000 alignment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, does the size value specified in the CSF script "[Authenticate Data]&lt;/P&gt;&lt;P&gt;Block =" command reflect the u-boot image size before or after padding?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: We are using the HAB4 CSF Fast Authentication loading the images via&lt;/P&gt;&lt;P&gt;USB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jan 2016 17:58:34 GMT</pubDate>
    <dc:creator>SJA</dc:creator>
    <dc:date>2016-01-08T17:58:34Z</dc:date>
    <item>
      <title>iMX6UL HAB Questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-HAB-Questions/m-p/478545#M76060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the signed u-boot image be verified on the EVK without CLOSING the SoC&lt;/P&gt;&lt;P&gt;when loading via USB (mfgtools technique)? When attempting this I&lt;/P&gt;&lt;P&gt;consistently see HAB events with INV_ADDRESS CTX_AUTHENTICATION. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the binary CSF file created using the cst tool have to be padded to the&lt;/P&gt;&lt;P&gt;size specified with CONFIG_CSF_SIZE in the u-boot imximage.cfg file before&lt;/P&gt;&lt;P&gt;being appended to the u-boot image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the signed u-boot image need to be padded for 0x1000 alignment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, does the size value specified in the CSF script "[Authenticate Data]&lt;/P&gt;&lt;P&gt;Block =" command reflect the u-boot image size before or after padding?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: We are using the HAB4 CSF Fast Authentication loading the images via&lt;/P&gt;&lt;P&gt;USB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 17:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-HAB-Questions/m-p/478545#M76060</guid>
      <dc:creator>SJA</dc:creator>
      <dc:date>2016-01-08T17:58:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL HAB Questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-HAB-Questions/m-p/478546#M76061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Please refer to Appendix E (Freescale manufacturing tool) of &lt;/P&gt;&lt;P&gt;recent AN4581 release (Rev. 1, 10/2015) - how to prepare U-boot for &lt;BR /&gt;MFG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 04:32:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-HAB-Questions/m-p/478546#M76061</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-01-11T04:32:01Z</dc:date>
    </item>
  </channel>
</rss>