<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Using PWM outputs as clock source</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-PWM-outputs-as-clock-source/m-p/478491#M76045</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following may help&amp;nbsp; &lt;A href="https://community.nxp.com/thread/321056"&gt;i.MX6S CLKO1 does not output 32kHz.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Apr 2016 06:27:19 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-04-04T06:27:19Z</dc:date>
    <item>
      <title>Using PWM outputs as clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-PWM-outputs-as-clock-source/m-p/478490#M76044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are designing a custom HW using iMX6Q and one of our peripheral devices needs a clock source of 32.768 kHz. Can we supply this through one of the PWM I/O on iMX? If not what port can I use to supply a peripheral with a clock at this frequency?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 05:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-PWM-outputs-as-clock-source/m-p/478490#M76044</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2016-04-04T05:56:43Z</dc:date>
    </item>
    <item>
      <title>Re: Using PWM outputs as clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-PWM-outputs-as-clock-source/m-p/478491#M76045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following may help&amp;nbsp; &lt;A href="https://community.nxp.com/thread/321056"&gt;i.MX6S CLKO1 does not output 32kHz.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 06:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-PWM-outputs-as-clock-source/m-p/478491#M76045</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-04T06:27:19Z</dc:date>
    </item>
  </channel>
</rss>