<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 ttymxc1 (uart) not receiving datas</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478463#M76029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi i am new to this,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have two custom imx6DL boards.But only one difference between two boards(i.e board A is configured with SD1 and board B is configured with SD3).&lt;/P&gt;&lt;P&gt;So in uboot i changed for board B SD1 to SD3 and inmachine driver itself i changed to SD3.&lt;/P&gt;&lt;P&gt;Both boards are configured with same UART pins.(&lt;/P&gt;&lt;P&gt;MX6Q_PAD_SD3_DAT4__GPIO_7_1,&lt;/P&gt;&lt;P&gt;MX6Q_PAD_SD3_DAT5__UART2_TXD,)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is Board A receive datas from microcontroller properly through UART.&lt;/P&gt;&lt;P&gt;But Board B is not at all receiving datas through UART from microcontroller.&lt;/P&gt;&lt;P&gt;I probe the receiver pin.But its toggle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So whats the issue?how can i solve?&lt;/P&gt;&lt;P&gt;please help me to identify the issue..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards,&lt;/P&gt;&lt;P&gt;R.Giritharan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 09:37:44 GMT</pubDate>
    <dc:creator>giritharanr</dc:creator>
    <dc:date>2016-04-26T09:37:44Z</dc:date>
    <item>
      <title>ttymxc1 (uart) not receiving datas</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478463#M76029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi i am new to this,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have two custom imx6DL boards.But only one difference between two boards(i.e board A is configured with SD1 and board B is configured with SD3).&lt;/P&gt;&lt;P&gt;So in uboot i changed for board B SD1 to SD3 and inmachine driver itself i changed to SD3.&lt;/P&gt;&lt;P&gt;Both boards are configured with same UART pins.(&lt;/P&gt;&lt;P&gt;MX6Q_PAD_SD3_DAT4__GPIO_7_1,&lt;/P&gt;&lt;P&gt;MX6Q_PAD_SD3_DAT5__UART2_TXD,)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is Board A receive datas from microcontroller properly through UART.&lt;/P&gt;&lt;P&gt;But Board B is not at all receiving datas through UART from microcontroller.&lt;/P&gt;&lt;P&gt;I probe the receiver pin.But its toggle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So whats the issue?how can i solve?&lt;/P&gt;&lt;P&gt;please help me to identify the issue..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards,&lt;/P&gt;&lt;P&gt;R.Giritharan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 09:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478463#M76029</guid>
      <dc:creator>giritharanr</dc:creator>
      <dc:date>2016-04-26T09:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: ttymxc1 (uart) not receiving datas</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478464#M76030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anybody is there???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 11:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478464#M76030</guid>
      <dc:creator>giritharanr</dc:creator>
      <dc:date>2016-04-26T11:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: ttymxc1 (uart) not receiving datas</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478465#M76031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why do you configure the SD3_DAT4 pin for GPIO function? To make it work as UART RX pin, you have to configure it as UART2_RXD.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 12:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ttymxc1-uart-not-receiving-datas/m-p/478465#M76031</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-04-28T12:01:17Z</dc:date>
    </item>
  </channel>
</rss>