<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Questions regarding IMX6 Multimedia Framework</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Questions-regarding-IMX6-Multimedia-Framework/m-p/477623#M75855</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Enrique&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.2. "without multimedia framework” means not using video player or other high level&lt;/P&gt;&lt;P&gt;application.&lt;/P&gt;&lt;P&gt;3. from i.MX6DQ RM (for performance of MIPI-CSI2 interface):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum bandwidth of the interface is as follows:&lt;/P&gt;&lt;P&gt;• 200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for your case, as "16bit RG565 which is acceptable for us. That’s a 168Mpixels/s."&lt;/P&gt;&lt;P&gt;seems this is sufficient.&lt;/P&gt;&lt;P&gt;HDMI is able 1080p60, using kernel parameter video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Dec 2015 02:01:58 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-11T02:01:58Z</dc:date>
    <item>
      <title>Questions regarding IMX6 Multimedia Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-regarding-IMX6-Multimedia-Framework/m-p/477622#M75854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have the following questions regarding IMX6 capabilities:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;In the TRM, what is meant by “60 fps in unit test without multimedia framework”? &lt;/LI&gt;&lt;LI&gt;What is that multimedia framework referred to? Specs I found were a few years old. Cannot see to find anything newer.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22216i6BD574ED990FC2FE/image-size/large?v=v2&amp;amp;px=999" title="Image 1.png" alt="Image 1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. From the TRM we know that the iMX6 is capable of doing 1080p60 (max 240Mpixels/s) especially &lt;STRONG&gt;for 1 cycle/pixel mode&lt;/STRONG&gt;. That would be 16bit RG565 which is acceptable for us. That’s a 168Mpixels/s. Can the iMX6 indeed support uncompressed RGB565 video 1080p60 in from MIPI to HDMI output? No codec involved. I am asking since we are struggling to achieve that frame rate. We seem to be blocked around ~50fps…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22399iF1B3567211A07409/image-size/large?v=v2&amp;amp;px=999" title="Image 2.jpg" alt="Image 2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;4. I found this link here doing some research that seem to indicate 1080p60 is doable: &lt;A href="https://developer.ridgerun.com/wiki/index.php/Toshiba_TC358743_Linux_driver_for_iMX6"&gt;https://developer.ridgerun.com/wiki/index.php/Toshiba_TC358743_Linux_driver_for_iMX6&lt;/A&gt;&lt;/P&gt;&lt;P&gt;5. I also found this link about using the right Gstreamer plugins to achieve full 60fps &lt;A href="https://developer.ridgerun.com/wiki/index.php/Toshiba_TC358743_Linux_driver_for_iMX6"&gt;https://developer.ridgerun.com/wiki/index.php/Toshiba_TC358743_Linux_driver_for_iMX6&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Last time was the big EIM bus inquiry which ended up being a big letdown for us, &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG style="text-decoration: underline;"&gt;now we are seeking a plain confirmation that iMX6 can pass through uncompressed 1080p60 from MIPI IN to HDMI out&lt;/STRONG&gt;&lt;/SPAN&gt;… &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In advance, thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 19:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-regarding-IMX6-Multimedia-Framework/m-p/477622#M75854</guid>
      <dc:creator>enriqueencarnac</dc:creator>
      <dc:date>2015-12-10T19:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: Questions regarding IMX6 Multimedia Framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-regarding-IMX6-Multimedia-Framework/m-p/477623#M75855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Enrique&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.2. "without multimedia framework” means not using video player or other high level&lt;/P&gt;&lt;P&gt;application.&lt;/P&gt;&lt;P&gt;3. from i.MX6DQ RM (for performance of MIPI-CSI2 interface):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum bandwidth of the interface is as follows:&lt;/P&gt;&lt;P&gt;• 200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for your case, as "16bit RG565 which is acceptable for us. That’s a 168Mpixels/s."&lt;/P&gt;&lt;P&gt;seems this is sufficient.&lt;/P&gt;&lt;P&gt;HDMI is able 1080p60, using kernel parameter video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Dec 2015 02:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-regarding-IMX6-Multimedia-Framework/m-p/477623#M75855</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-11T02:01:58Z</dc:date>
    </item>
  </channel>
</rss>