<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6SX: VADC &amp; CPU load in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477584#M75820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you confim if high cpu loading is caused by only playing video?&lt;/P&gt;&lt;P&gt;high cpu loading depends on what usage cpu use.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Apr 2016 07:59:43 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2016-04-28T07:59:43Z</dc:date>
    <item>
      <title>iMX6SX: VADC &amp; CPU load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477583#M75819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the VADC of the iMX6 SoloX (Sabre board) to capture and show an analog camera signal with following Gstreamer pipeline:&lt;/P&gt;&lt;P&gt;&lt;EM style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0 &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pipeline works, i.e. the picture is shown correctly, but I get a CPU load of nearly 100% while the pipeline is running, which, of course, is not acceptable. I would expect a one-digit cpu-load. What am I doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using kernel 4.1.x.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 09:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477583#M75819</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2016-04-26T09:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX: VADC &amp; CPU load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477584#M75820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you confim if high cpu loading is caused by only playing video?&lt;/P&gt;&lt;P&gt;high cpu loading depends on what usage cpu use.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 07:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477584#M75820</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-04-28T07:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX: VADC &amp; CPU load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477585#M75821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I can confirm that; &lt;EM&gt;gst-launch&lt;/EM&gt; is eating up all the cpu-cycles. When I terminate the process, the cpu-load is close to 0%.&lt;/P&gt;&lt;P&gt;I'm pretty sure you can easily repdroduce this behavior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 08:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477585#M75821</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2016-04-28T08:06:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX: VADC &amp; CPU load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477586#M75822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how about add "sync=false " in the command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 08:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477586#M75822</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-04-28T08:37:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX: VADC &amp; CPU load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477587#M75823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've tried with &lt;EM&gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0 sync=false&lt;/EM&gt; and still the same result (output from top):&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;PID&amp;nbsp; PPID USER&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STAT&amp;nbsp;&amp;nbsp; VSZ %VSZ %CPU COMMAND&lt;/P&gt;&lt;P&gt;597&amp;nbsp;&amp;nbsp; 568 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; S&amp;nbsp;&amp;nbsp;&amp;nbsp; 52064&amp;nbsp;&amp;nbsp; 5%&amp;nbsp; 99% gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0 sync=false&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I've also tried to set the sync property on the imxv4l2src, but the property apparently does not exist there.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 08:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-CPU-load/m-p/477587#M75823</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2016-04-28T08:47:26Z</dc:date>
    </item>
  </channel>
</rss>