<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Yocto .sdcard image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477465#M75769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi &lt;/P&gt;&lt;P&gt;I want to modify Yocto .sdcard image for my custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which file needs to modify to change .sdcard image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 04:10:44 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2016-04-26T04:10:44Z</dc:date>
    <item>
      <title>Yocto .sdcard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477465#M75769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi &lt;/P&gt;&lt;P&gt;I want to modify Yocto .sdcard image for my custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which file needs to modify to change .sdcard image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 04:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477465#M75769</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2016-04-26T04:10:44Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto .sdcard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477466#M75770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You need to rebuild Your project.&lt;/P&gt;&lt;P&gt;Please refer to the following :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389283"&gt;How to modify yocto jethro and rebuild&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/376214"&gt;How to modify source code and rebuild yocto project?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 04:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477466#M75770</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-26T04:26:04Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto .sdcard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477467#M75771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;I have yocto build ready.&lt;/P&gt;&lt;P&gt;I want to prepare .sdcard image that include u-boot, uImage, dtb , rootfs, bmp logo and additional script.&lt;/P&gt;&lt;P&gt;I want to include bmp logo and additional script in yocto build, so whenever I build Yocto build I get final image.&lt;/P&gt;&lt;P&gt;So I need to modify sdcard image generation&amp;nbsp; to include additional files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 04:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477467#M75771</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2016-04-26T04:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto .sdcard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477468#M75772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may mount the image file using "-o loop" option and treat&amp;nbsp; it as&lt;/P&gt;&lt;P&gt;file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 06:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477468#M75772</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-26T06:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto .sdcard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477469#M75773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saurabh,&lt;/P&gt;&lt;P&gt;To add custom scripts and files, create a new meta layer of your own or create a new recipe on existing meta-*/recipr-*/ directory (refer other recipe to get reference), add your files and also add a bb file for the same. Now specify the name of bb file on the image which you are building. Better to create a new layer, refer section 5.1.8 in the link below to know how layers are created.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/1.8/dev-manual/dev-manual.html#creating-a-general-layer-using-the-yocto-layer-script" title="http://www.yoctoproject.org/docs/1.8/dev-manual/dev-manual.html#creating-a-general-layer-using-the-yocto-layer-script"&gt;Yocto Project Development Manual&lt;/A&gt;​&lt;/P&gt;&lt;P&gt;Also add the name of your bb file in the image file (eg: images/core-image-minimal.bb etc)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 13:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-sdcard-image/m-p/477469#M75773</guid>
      <dc:creator>pranavmadhu</dc:creator>
      <dc:date>2016-07-19T13:00:49Z</dc:date>
    </item>
  </channel>
</rss>