<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 standalone in u-boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/standalone-in-u-boot/m-p/477449#M75762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;I.mx community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have written an application and compiled with arm-none-eabi tools with own make file&lt;/P&gt;&lt;P&gt;the start address is 0x12000000 which is also set in linker script.&lt;/P&gt;&lt;P&gt;i am downloading to 0x12000000 address on sabresd board and trying to run it but i am getting " application terminated " 0xfb, error&lt;/P&gt;&lt;P&gt;am doing this in wrong way&lt;/P&gt;&lt;P&gt;can any one give me the right procedure to do it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks and regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Dec 2015 11:10:04 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2015-12-11T11:10:04Z</dc:date>
    <item>
      <title>standalone in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/standalone-in-u-boot/m-p/477449#M75762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;I.mx community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have written an application and compiled with arm-none-eabi tools with own make file&lt;/P&gt;&lt;P&gt;the start address is 0x12000000 which is also set in linker script.&lt;/P&gt;&lt;P&gt;i am downloading to 0x12000000 address on sabresd board and trying to run it but i am getting " application terminated " 0xfb, error&lt;/P&gt;&lt;P&gt;am doing this in wrong way&lt;/P&gt;&lt;P&gt;can any one give me the right procedure to do it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks and regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Dec 2015 11:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/standalone-in-u-boot/m-p/477449#M75762</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-12-11T11:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: standalone in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/standalone-in-u-boot/m-p/477450#M75763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uboot runs standalone application as procedure, not as OS,&lt;/P&gt;&lt;P&gt;so this may be caused by stack misconfiguration, example of&lt;/P&gt;&lt;P&gt;standalone application:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.denx.de/wiki/view/DULG/UBootStandalone" rel="nofollow"&gt;http://www.denx.de/wiki/view/DULG/UBootStandalone&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://stackoverflow.com/questions/21622762/uboot-terminate-standalone-application" rel="nofollow"&gt;http://stackoverflow.com/questions/21622762/uboot-terminate-standalone-application&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Dec 2015 09:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/standalone-in-u-boot/m-p/477450#M75763</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-12T09:14:31Z</dc:date>
    </item>
  </channel>
</rss>