<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: error: output DMA task timeout in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477425#M75759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi akk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems one will have custom application for such task, refer to&lt;/P&gt;&lt;P&gt;sect.30.2.1 Sequence for Memory to ASRC to Memory attached Linux Manual.&lt;/P&gt;&lt;P&gt;Currently implemented only Sequence for Memory to ASRC to Peripheral, as&lt;/P&gt;&lt;P&gt;described in sect.30.2.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jan 2016 01:56:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-01-12T01:56:24Z</dc:date>
    <item>
      <title>error: output DMA task timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477424#M75758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using imx6 ul evk.&lt;/P&gt;&lt;P&gt;I want to use hardware asrc on imx board to convert sampling rate of decoded bit streams into one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The input to ASRC is pcm array.&lt;/P&gt;&lt;P&gt;when i execute , it shows following error and did not generate any output :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;output DMA task timeout&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;fsl-asrc 2034000.asrc: Pair A: failed to process buffer: -62&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kindly help me to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 06:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477424#M75758</guid>
      <dc:creator>akk1</dc:creator>
      <dc:date>2016-01-11T06:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: error: output DMA task timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477425#M75759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi akk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems one will have custom application for such task, refer to&lt;/P&gt;&lt;P&gt;sect.30.2.1 Sequence for Memory to ASRC to Memory attached Linux Manual.&lt;/P&gt;&lt;P&gt;Currently implemented only Sequence for Memory to ASRC to Peripheral, as&lt;/P&gt;&lt;P&gt;described in sect.30.2.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 01:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477425#M75759</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-12T01:56:24Z</dc:date>
    </item>
    <item>
      <title>Re: error: output DMA task timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477426#M75760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor, do you know any sample code implementation of hardware asrc in imx6ul for two simultaneous conversions. For example, I want to convert 5 channels&amp;nbsp; from sampling rates 44100 Hz to 48000 Hz. Another 5 channels for 48000 Hz to 96000 Hz. As far as I know there are atmost 10 channels with three simultaneous pair conversions are possible in imx6ul. Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 15:44:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477426#M75760</guid>
      <dc:creator>phanikumar</dc:creator>
      <dc:date>2016-01-12T15:44:20Z</dc:date>
    </item>
    <item>
      <title>Re: error: output DMA task timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477427#M75761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A few years after, have you resolved your issue ? I am running into the exact same one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Julien.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 13:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/error-output-DMA-task-timeout/m-p/477427#M75761</guid>
      <dc:creator>JulienP</dc:creator>
      <dc:date>2020-07-20T13:48:26Z</dc:date>
    </item>
  </channel>
</rss>