<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: File transfer between imx28 and host PC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476640#M75604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use use z-modem protocol in the terminal you are using to connect the board.&lt;/P&gt;&lt;P&gt;First you need to connect the board and run "rz" utility. It will wait for the file to be sent.&lt;/P&gt;&lt;P&gt;Then you need to transfer the file from the terminal.&lt;/P&gt;&lt;P&gt;For example in minicom you need to press Ctrl+A and Z and then S for this option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Mar 2016 08:44:05 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-03-15T08:44:05Z</dc:date>
    <item>
      <title>File transfer between imx28 and host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476639#M75603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello mates!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm quite noob with the imx28 evaluation board. I've been able to flash a kernel to a SD card and boot from there. Also I've been able to log to the board using RS232 terminal. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to install java and transfer some files from my host PC to the board. Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 07:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476639#M75603</guid>
      <dc:creator>alexaldridge</dc:creator>
      <dc:date>2016-03-15T07:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: File transfer between imx28 and host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476640#M75604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use use z-modem protocol in the terminal you are using to connect the board.&lt;/P&gt;&lt;P&gt;First you need to connect the board and run "rz" utility. It will wait for the file to be sent.&lt;/P&gt;&lt;P&gt;Then you need to transfer the file from the terminal.&lt;/P&gt;&lt;P&gt;For example in minicom you need to press Ctrl+A and Z and then S for this option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 08:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476640#M75604</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-03-15T08:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: File transfer between imx28 and host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476641#M75605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the suggestion. If I do rz in my mx28 I get: "rz not found".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 09:05:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476641#M75605</guid>
      <dc:creator>alexaldridge</dc:creator>
      <dc:date>2016-03-15T09:05:44Z</dc:date>
    </item>
    <item>
      <title>Re: File transfer between imx28 and host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476642#M75606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may try using WinSCP on Windows host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 02:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/File-transfer-between-imx28-and-host-PC/m-p/476642#M75606</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-03-16T02:26:21Z</dc:date>
    </item>
  </channel>
</rss>