<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RAM size in Linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476229#M75564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After setting:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;#define PHYS_SDRAM_SIZE (1u * 480 * 1024 * 1024)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;u-boot still shows:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;U-Boot 2015.07 (Apr 26 2016 - 13:05:59 +0200)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.5 at 792MHz&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Industrial temperature grade (-40C to 105C) at 53C&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: MX6&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DRAM:&amp;nbsp; 512 MiB&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x10&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;Using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x61dcb0 ]&lt;/P&gt;&lt;P&gt;## Loading init Ramdisk from Legacy Image at 12c00000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux RAMDisk Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 31276561 Bytes = 29.8 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 18000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x18000000&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; Loading Ramdisk to 2d785000, end 2f558e11 ... OK&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; Loading Device Tree to 2d779000, end 2d784cc2 ... OK&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 11:11:50 GMT</pubDate>
    <dc:creator>jotes</dc:creator>
    <dc:date>2016-04-26T11:11:50Z</dc:date>
    <item>
      <title>RAM size in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476227#M75562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to reduce amount of memory which can be accessed by Linux? Adding&amp;nbsp; "memory" part to devicetree or "mem=" argument to the kernel command line doesn't work. Is there any other way? I am using IMX6Q with the following software: buildroot-2015.11.1, linux-imx6-boundary-imx_3.14.38_6qp_ga-pass1, u-boot-2015.07.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 07:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476227#M75562</guid>
      <dc:creator>jotes</dc:creator>
      <dc:date>2016-04-26T07:06:04Z</dc:date>
    </item>
    <item>
      <title>Re: RAM size in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476228#M75563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jotes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for setting memory size in linux one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="http://stackoverflow.com/questions/13484016/setting-limit-to-total-physical-memory-available-in-linux" title="http://stackoverflow.com/questions/13484016/setting-limit-to-total-physical-memory-available-in-linux"&gt;http://stackoverflow.com/questions/13484016/setting-limit-to-total-physical-memory-available-in-linux&lt;/A&gt; &lt;/P&gt;&lt;P&gt;or try to set in uboot/include/configs/board_file parameter #define PHYS_SDRAM_SIZE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 09:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476228#M75563</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-26T09:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: RAM size in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476229#M75564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After setting:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;#define PHYS_SDRAM_SIZE (1u * 480 * 1024 * 1024)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;u-boot still shows:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;U-Boot 2015.07 (Apr 26 2016 - 13:05:59 +0200)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.5 at 792MHz&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Industrial temperature grade (-40C to 105C) at 53C&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: MX6&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DRAM:&amp;nbsp; 512 MiB&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x10&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;Using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x61dcb0 ]&lt;/P&gt;&lt;P&gt;## Loading init Ramdisk from Legacy Image at 12c00000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux RAMDisk Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 31276561 Bytes = 29.8 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 18000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x18000000&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; Loading Ramdisk to 2d785000, end 2f558e11 ... OK&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; Loading Device Tree to 2d779000, end 2d784cc2 ... OK&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 11:11:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-size-in-Linux/m-p/476229#M75564</guid>
      <dc:creator>jotes</dc:creator>
      <dc:date>2016-04-26T11:11:50Z</dc:date>
    </item>
  </channel>
</rss>